Toshiba Satellite L655-S5155 Laptop

Satellite L655-S5155

MSRP: $579.99
Satellite L655-S5155 4.17 out of 5.0 based on 34 user reviews. Average Customer Rating: 4.17 out of 5.0
Read Reviews (34) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Satellite L850 Series »
Laptop Accessories
Shop for Satellite L655-S5155 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L655-S5155 or try our Laptop Forums for additional help.
Intel® Pentium® Processor
Accessories for the Satellite L655-S5155

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L655-S5155 Laptop Customer Reviews

Amazing Laptop!

POSTED BY: , raleigh, nc
Overall rating: 5.0 out of 5

"amazing design, fast, full keyboard, and lots of memory"

a good replacement for my old dinosaur!

POSTED BY: , brighton, MA
Overall rating: 4.0 out of 5

"This is a major improvement over my old Toshiba purchased in 2003. So much faster at half the price. I do not have to waste so much time WAITING. It's also easier to use."

Great purchase

POSTED BY:
Overall rating: 5.0 out of 5

"This model had all the features that I wanted. And it was the right color too!"

Really great

POSTED BY: , Marriottsville, MD
Overall rating: 5.0 out of 5

"Very Good,"

My Feelings about Toshiba

POSTED BY: , Phoenix, AZ
Overall rating: 4.0 out of 5

"I love the feel of the keys and it is responsive and since I was an accountant I love the number keypad for the feel of a full size keypad. Still getting used to the placing of the delete key, etc."

Best Value For Dollar Spent

POSTED BY: , Manchester, NH
Overall rating: 4.0 out of 5

"I was attracted to this product for the incredible amount of computing power, for the sticker price advertised. The physical package is slick and handsome. I can access almost any media source with little or no further investing in hardware. This has opened a whole new world of information availiblity and connectivity to millions of data resources and ideas."

Love This Laptop!

POSTED BY: , Brooklyn, NY
Overall rating: 5.0 out of 5

"Much better than any of my HP's!"

Have had better luck with an older Toshiba

POSTED BY: , Fulton,NY
Overall rating: 2.0 out of 5

"I have a 2 year old Toshiba Satellite with an Intel Dual Core processor that opens applications faster than this one. The mouse touch pad is flaky. Need to touch it close to center for it work. Battery life does not make the 5 hours as mentioned."

TOUCHPAD IS LOUSY

POSTED BY: , WEMOUTH MA
Overall rating: 4.0 out of 5

"I AM VERY HAPPY WITH THIS COMPUTER WITH 1 EXCEPTION, I DO NOT LIKE THE TOUCHPAD, IT DOES NOT RESPOND THE SAME TWICE, IT REALLY NEEDS TO BE IMPROVED"

Beat Laptop for the Money

POSTED BY: , Rolla, MO
Overall rating: 5.0 out of 5

"I would never go back to my stationary desktop after using this laptop. It has a great keyboard and a perfect display with super fast computing. It is loaded with built-in features from web camera to wireless internet connection. A very high quality to price ratio."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.