POSTED BY:
Toby
,
Rio Rancho, NM
Overall rating:
4.0 out of 5
"Works well for what it is. Great for web surfing, not for gaming. Needs a bit more RAM for my occasional game playing on Facebook. Stylish in design, screen sharp."
POSTED BY:
Neros
Overall rating:
4.0 out of 5
"Overall its a pretty good laptop. Only main problems I have with it is the sound. Even with the audio program helping it, it still sounds bad from the speakers and headphones. Lack low end sounds and is mostly high pitched sounds and slightly echoy sounding. Also the battery life seems to go anywhere from 2-4 hours depending on screen brightness and what you doing on it."
POSTED BY:
azbohnt
,
az
Overall rating:
4.0 out of 5
"kEY BOARD NEEDS SOME WORK / REFINEMENT AND THE MOUSE NEEDS TO BE PLACED IN A DIFFERENT LOCATION TOO MANY TIMES SO FAR LOST INFORMATION FOR SCHOOL BECAUSE THE KEY BOARD IS IN GTHE WAY OF MY HANDS AND DELETES AND THEN SAVES THE INFORMATION BEFORE YOU CAN DO ANYTHING TO PRVENT IT."
POSTED BY:
toolman
,
U.S.A.
Overall rating:
3.0 out of 5
"I think the keyboard layout is poor and the keys take up too much space and the layout could be smaller. The touch pad is too sensitive. Features I have seen are decent, but I am truly still learning it."
POSTED BY:
mikeman
,
Michigan
Overall rating:
5.0 out of 5
"Only had it a month but overall very nice good weight, looks nice, its fast. I wish the battery life was longer with continuous use its about an hour but if just using off and on it last almost all day nice power saving features to prolong battery life. Only one irritation is the power cord plugs in on the side I really prefer if it was in the rear of the machine"
POSTED BY:
Tikiman
Overall rating:
3.0 out of 5
"Mouse is extremely sensitive. However, keyboard responds well and it is a quiet machine. I'm disappointed that I don't seem to have a CD/DVD burner and I abhor Windows 7. Size and weight are satisfactory."
POSTED BY:
* MISS DIRTY RED * WOOT WOOT
,
E-LOY, ARIZONA
Overall rating:
5.0 out of 5
"THE LAPTOP IS PRETTY DARN FAST A 500 GIG DRIVE , LIGHT WEIGHT, AND REASONABLE PRICE. WHY LET AN OFFER LIKE THIS SLIP BY ? THE ONLY NEGATIVE THING IS THE FAN, IT IS WAY TOO LOUD !! THE BATTERY LIFE DOESN'T LAST AS ADVERTISED. OH ! AND ONE MORE THING IT DOES NOT HAVE A BUILT-IN WEBCAM WHICH IS ALSO ADVERTISED ON (SKYPE STICKER) SO DONT BE FOOLED AND OVERLOOK IT AS I DID. OTHER THAN THAT ITS OVER ALL PERFORMANCE IS GOOD."
POSTED BY:
((Az Mami))
,
E-Town,AZ
Overall rating:
5.0 out of 5
"Good for on the go or @ home laptop. It's light weight & reasonable price :o) If only it had a built-in webcam as the majority of laptops do. You couldn't ask for more, other than that i love it ! "Go Toshiba""
POSTED BY:
Bird
,
Chicago, IL
Overall rating:
5.0 out of 5
"The only thing negative about the laptop is that the battery does not last as long as advertised. Otherwise than that, it's light, the keypad is very easy to use and it's overall appearance is very nice."
POSTED BY:
dazecuttiebaby
,
Baldwin Park, CA
Overall rating:
4.0 out of 5
"The only bad thing about the laptop is that the fan is too loud. Aside from that it's a great product for the price."