Toshiba Satellite L750-ST5N02 Laptop

Satellite L750-ST5N02

MSRP: $849.00
Satellite L750-ST5N02 4.25 out of 5.0 based on 8 user reviews. Average Customer Rating: 4.25 out of 5.0
Read Reviews (8) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L750-ST5N02 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L750-ST5N02 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite L750-ST5N02

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L750-ST5N02 Laptop Customer Reviews

Didn't Work

POSTED BY:
Overall rating: 1.0 out of 5

"The laptop didn't work out of the box due to hardware failure."

Very good lap top, I have three Lap top Toshibas

POSTED BY: , Fl.
Overall rating: 5.0 out of 5

"I would buy another Toshiba if need be. They are very dependable and run like clock work. I never shut them down,and they awaken quick ready to go."

Solid laptop

POSTED BY: , Hobart, Indiana
Overall rating: 5.0 out of 5

"I use the laptop for running all the usual programs, however I also run many virtual machines on it as well. I use virtualization quite a bit. Rather than keep restoring my laptop I just simply create a virtual machine to test and then toss it away when I'm done or use them to run specific apps with specific hardware/configuration needs. However, it is a little slow with running both a virtual machine and a web browser. I should have gone with the i7."

Powerful Laptop

POSTED BY: , Fort Lauderdale
Overall rating: 5.0 out of 5

"From the time I open the box, to have the L7 50 fully operational was 30 min. With Toshiba support connecting for upgrades, the laptop was fully operational within another 30 min. With the new i7 core, it's a very powerful machine particularly when I added 512 Gb SSD drive. This is just an outstanding laptop."

Good laptop

POSTED BY:
Overall rating: 4.0 out of 5

"This is a good laptop for the money. I have used it to make phone calls with Bluetooth over VOIP. I have noticed when running a VM machine the unit slows down. More memory should help here."

Can't beat Toshiba

POSTED BY: , Peoria, AZ
Overall rating: 5.0 out of 5

"Toshiba makes great laptops. My last one went 5 years without a problem. It had traveled the world several times so it had been put through the ringers. Couldn't ask for more."

good value

POSTED BY: , nyc
Overall rating: 4.0 out of 5

"fast, reliable, good screen and service. sound could be better"

Best I have ever owned

POSTED BY: , Katy, TX
Overall rating: 5.0 out of 5

"This is my 3rd Toshiba in over 10 years. I love the machines and they last almost forever. The L750-ST5N02 is awesome. The speed, memory, hard drive are all great, especially for the money. The full size, 10key keyboard sure makes my life easier."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.