Toshiba Satellite L750-ST6N01 Laptop

Satellite L750-ST6N01

MSRP: $849.99
Satellite L750-ST6N01 4.29 out of 5.0 based on 7 user reviews. Average Customer Rating: 4.29 out of 5.0
Read Reviews (7) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L750-ST6N01 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L750-ST6N01 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite L750-ST6N01

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L750-ST6N01 Laptop Customer Reviews

Good Value

POSTED BY: , Arcadia
Overall rating: 5.0 out of 5

"It was the best price for the features I wanted for a laptop including processing speed, memory and software. Delivery was quick too. Only minus was both the keyboard rest and cover scratch easily. :-("

Very Pleased!

POSTED BY: , Kuna, ID
Overall rating: 5.0 out of 5

"I wanted a laptop so I could pursue my writing goals without having to share the family computer with my husband and 4 kids. I've been very happy with this machine!"

Don't buy this one

POSTED BY: , Pensacola, FL
Overall rating: 1.0 out of 5

"Bought this lap top based on my Sister having one also and she loves it. I got a dog of a computer that doesn't like to connect to wifi, is painfully slow, fully charged battery is about a 2 hour life span, lid is hard to lift up."

Awesome Laptop!

POSTED BY: , meridian, ms
Overall rating: 5.0 out of 5

"This laptop has it all. Looks, Speed, Performance, Reliability, Features and at a very great price. Other brands with these features would cost much more."

Great Lapton

POSTED BY: , Tucson AZ
Overall rating: 5.0 out of 5

"This is 4th Toshiba laptop I have had and is the best yet. It is light, it is responsive and has has great battery life! I don't feel I need to be tied to an electric plug!"

POSTED BY: , Illinois
Overall rating: 4.0 out of 5

"Several annoyances. The hinge on the lid is so tight that it cannot be opened with one hand without lifting up the bottom half from the table, only for it to then slam down once the lid passes a certain point. Another is that connector for the slave monitor has no screw holes, so the connector tends to fall out. I reconnect it no less than 10 times a day and I fear that it will wear out the connector itself. Performance is slower than I thought it would be. Takes far longer to load a program than it should and all that I am running is Word, explorer, out look. This is my third Toshiba over the years and the only one I dont care for."

Very nice laptop

POSTED BY: , solomons MD
Overall rating: 5.0 out of 5

"Received notebook in good order, it was easy to get it going, and with an hour I was totally set up to use all functions of the unit."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.