POSTED BY:
Ed
,
Baltimore, MD
Overall rating:
5.0 out of 5
"Works very well. It's fast, has everything that I need. The features are as good as any top brand laptop. I made a very good decision to purchase this computer."
POSTED BY:
Eileen
,
Trenton, Fl
Overall rating:
4.0 out of 5
"I have not tried using the battery, so I'm not able to rate it. So far at 3 months, this laptop is performing to expectations. However, I was told I could record from the TV. This is not true, unless someone has found a convenient way to do it. I have a Toshiba with windows XP and I connect it to a capture box connected to my satellite receiver. But my capture device will not work with windows 7 and newer capture devices that do only record to hard drive in MPEG2 or DVD quality instead of a choice of several compressions. So most features on this computer will be rarely used."
POSTED BY:
none
,
Satsuma, FL
Overall rating:
5.0 out of 5
"So far it has been the best laptop I have owned. It is very fast and very reliable."
POSTED BY:
Nick
,
Ottawa, Ontario
Overall rating:
5.0 out of 5
"I have only one suggestion and that is in the location of the USB ports on the extreme right hand lower corner, they are a bit ackward there if you are using an external mouse in cramped conditions as you have a tendency to bump them."
POSTED BY:
Cactus
,
Tucson, AZ
Overall rating:
5.0 out of 5
"I have been shopping for a computer since November 2011. I read reviews and if the review has something negative that I cannot handle as I am not an expert, then I do not consider the computer. When I find good reviews, I take the spec's to my experts. This computer had minimal ...I mean minimal negative reviews, it had everhthing I wanted and my experts gave it a thumbs up on the the things they looked for. The cost was in my range and my search was over. I am highly satisfied with this computer."
POSTED BY:
Pcta
,
Albuquerque, nm
Overall rating:
3.0 out of 5
"Perhaps it is merely an issue with this particular box. I will be calling support next week. The battery indicator told me I had over 2 hours left on battery life with an 80% charge - 10 min later the machine turned off because of low battery and when I stuck in the AC adaptor battery charge was less than 15%. This is my 3rd Toshiba laptop and except for the battery issue it is as good as the previous editions."
POSTED BY:
school boy
,
Rochester, Mn
Overall rating:
4.0 out of 5
"its a great laptop only problem I have is the mouse pad is slow sometimes and it malfunctions i think there is a bug in the drivers."
POSTED BY:
champion
,
Bing , NY
Overall rating:
5.0 out of 5
"I am glad that my new laptop is very well good quality . i like toshiba more than dell laptop"
POSTED BY:
thanatos423
,
Sacramento, CA
Overall rating:
4.0 out of 5
"I had a dead pixel, it's off to the left and hard to notice. I decided to keep it because I didn't want to send it back and all that, but it's the best laptop I have ever owned. I would still recommend a Toshiba."
POSTED BY:
HB
Overall rating:
5.0 out of 5
"Excellent versatile laptop. I am very pleased with my purchase. I will be buying another for a family member within the next 12 months."