Toshiba Satellite L755-S5112 Laptop

Satellite L755-S5112

MSRP: $550.99
Satellite L755-S5112 4.42 out of 5.0 based on 12 user reviews. Average Customer Rating: 4.42 out of 5.0
Read Reviews (12) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5112 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5112 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor

Satellite L755-S5112 Laptop Customer Reviews

One great laptop

POSTED BY: , Ocala, Florida
Overall rating: 5.0 out of 5

"At first i bought a Toshiba laptop with the pentium chip..i had trouble with it, and took it back..it had the 15 inch screen.... I returned it for the 17 inch screen, and the AMD chip and love it...it runs super fast...its more computer then i need...i highly recommend it..."

not happy with screen

POSTED BY: , pembroke ma
Overall rating: 3.0 out of 5

"I am not satisfied with the quality and color of the screen images. My hp laptop screen was much clearer with sharp colors."

My First Toshiba

POSTED BY: , NSB Florida
Overall rating: 5.0 out of 5

"I have owned a number of laptops and desktops and this the first time I have purchased a Toshiba. I am very glad I did. It is a great machine. Very fast, easy to carry and great features."

SAtellite Scores!

POSTED BY: , Berwyn, PA
Overall rating: 4.0 out of 5

"This computer works like a charm with easy and fast performance- and at a great price!. I wish there was a clasp to close the lid instead of having it loosely closed in my bag."

First laptop I've owned.

POSTED BY: , Tucson, AZ
Overall rating: 4.0 out of 5

"I like it very much,but I haven't used it on the go yet."

Awesome Toshiba

POSTED BY: , Mount Dora, FL
Overall rating: 5.0 out of 5

"First time I use Toshiba laptop when it was amazing and smooth internet and everything there. The battery life is very good longer and it let me know how many hours that so cool!! I compared Toshiba better much tech than HP. I feel comfortable with Toshiba laptop."

Great unit

POSTED BY: , Providence,
Overall rating: 4.0 out of 5

"easy to set up and transfer old files to new laptop. Great value"

Nice laptop for the price

POSTED BY: , Massachusetts
Overall rating: 4.0 out of 5

"I needed a new laptop for email and downloading lesson plans for my students. This laptop fell in my price range and has a sleek design."

Very Happy

POSTED BY: , Plantation, Fl
Overall rating: 5.0 out of 5

"I am very happy with my Toshiba, this is the best computer I have owned yet. I have had other brands and this one is the one I found no flaws with so far. I would recommend it."

Satellite L755

POSTED BY: , Denver CO
Overall rating: 4.0 out of 5

"I was in the market for a new laptop and wanted something functional, reasonably priced, and portable. I did not need the maximum performance and also had a budget. The Toshiba met all my criteria in a very reasonably priced product! I will probably upgrade to 8gb memory (from 2) to (hopefully) speed things up a bit but overall I am VERY happy with this laptop!"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.