Toshiba Satellite L755-S5166 Laptop

Satellite L755-S5166

MSRP: $599.99
Satellite L755-S5166 4.60 out of 5.0 based on 5 user reviews. Average Customer Rating: 4.60 out of 5.0
Read Reviews (5) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5166 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5166 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite L755-S5166

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L755-S5166 Laptop Customer Reviews

Great Laptop

POSTED BY: , Sidney, Ohio
Overall rating: 4.0 out of 5

"Love my new laptop. It is very fast. I do plan to upgrade it to 8G of memory, the cost to do this is very cheap. It is a little noisy compared to my other laptop which is also a Toshiba, but not enough that I would not recommend it to others."

Beautiful Laptop

POSTED BY: , Cincinnati, Ohio
Overall rating: 5.0 out of 5

"I am so happy with my purchase. This laptop is fast, runs cool enough to use on my lap, and has a nice wide viewing for sharing movies with family on the couch! It was shutting itself down unexpectedly the first few times I used it, but I believe I have corrected that, and have no other problems!"

Love it!

POSTED BY: , Anywhere, USA
Overall rating: 5.0 out of 5

"I bought this to replace a burned out netbook. Maybe it is just because of the difference in performance between the two platforms, but this thing has exceeded my expectations! Using it in an area with limited connectivity, the connection is always strong and the processor flies. Programs open quickly and without fail. I would definitely recommend this to a friend!"

Good Laptop @ Good Price

POSTED BY: , Torrance, CA
Overall rating: 4.0 out of 5

"I just needed a basic laptop to do basic photo editing (non-professional) for my volunteer work. As well as standard emailing and internet surfing. So far I've had no issues with the computer other than I wish it had longer battery life. I have always had a desktop and felt that I should switch to a laptop. So far I'm really happy with my new computer."

LIke it very much.

POSTED BY: , Fargo, ND
Overall rating: 5.0 out of 5

"I really like the user friendly ability of this laptop. The processing power is great for what I need it for."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.