Toshiba Satellite L755-S5175 Laptop

Satellite L755-S5175

MSRP: $729.99
Satellite L755-S5175 4.33 out of 5.0 based on 12 user reviews. Average Customer Rating: 4.33 out of 5.0
Read Reviews (12) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5175 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5175 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite L755-S5175

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L755-S5175 Laptop Customer Reviews

Nice Machine

POSTED BY: , Rock Hill, SC
Overall rating: 5.0 out of 5

"So far this machine has lived up to what I expected it to be. I like the fact that it is quiet. Only two minor points. It does not sleep all the time when the lid is closed and I wish it had some more contrast."

having some problems

POSTED BY: , lewiston, id
Overall rating: 4.0 out of 5

"this PC is having trouble with the internet. the internet goes down often and I don't know what to do-maybe the internet connection just fails but I don't know if it is the machine or internet. the PC works well otherwise."

Nice kepad

POSTED BY: , Sumner Wa.
Overall rating: 4.0 out of 5

"I like the size of the key board. The keys are big enogh for my fingers so it is easyer for me to type."

Laptop or desktop?

POSTED BY:
Overall rating: 4.0 out of 5

"I had a simple criteria: My next computer would need to perform as well as an average desktop. The Satellite laptop has performed as needed. It can easily handle multiple tasks; open browser windows and programs -installation and use. HDMI port to TV screen, two USB 2.0 and (one) 3.0 handle all my needs. The standard battery life is adequate - about 3 hours including a USB-powered exterior fan. I couldn't comment on how this model would perform for a graphics-intensive user, but for business and "standard" home use, it will suit me well."

It is getting the job done

POSTED BY: , Currituck, NC
Overall rating: 4.0 out of 5

"It may not be fair for me to write a lot since I'm not computer savy. I would however like to know where the heck spell check is located, can't seem to find it."

Great Laptop

POSTED BY: , West Linn, OR
Overall rating: 5.0 out of 5

"I have had this laptop for 2 months. I havent had any issues so far. It is a great value for the money."

Very Good Value

POSTED BY: , MI
Overall rating: 4.0 out of 5

"I always purchased HP computers and I like this for the value for the $ spent. I am still getting used to the differences between HP and my new T. Keys are slippery, a few placement differences and not contoured like other lap tops and desk tops I have used. A bit of noise from the hard drive and I feel vibration a too. A bit of a concern at the moment. Like the speed, screen size, built in mic and video camera."

Love IT!

POSTED BY: , Indianapolis, IN
Overall rating: 5.0 out of 5

"It runs fast, is easy to use, has a great operating system - what more can you ask for?"

Great machine

POSTED BY: , Acworth, Ga
Overall rating: 5.0 out of 5

"This laptop is outstanding. It has all the features I wanted, loads quickly and came with the software I prefer."

nice laptop

POSTED BY: , San Diego, CA
Overall rating: 4.0 out of 5

"My only real complaints are with the cursor and touch pad. I have the jumping cursor which is totally aggravating, and seems to be no answer for. The touch pad is so extremely sensitive that I had to turn it down the whole way to keep text and blocks from continually lighting up. I have no idea why it does this but a real detriment. Lastly, dont understand this either but if I delete an email, it is likely one or two more nearby will delete also when I hit 'delete'. These things really hamper having an enjoyable experience with it, and I find myself not using it as much as I would like."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.