Toshiba Satellite L755-S5214 Laptop

Satellite L755-S5214

MSRP: $548.99
Satellite L755-S5214 4.31 out of 5.0 based on 51 user reviews. Average Customer Rating: 4.31 out of 5.0
Read Reviews (51) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5214 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5214 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite L755-S5214

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L755-S5214 Laptop Customer Reviews

Great Laptop

POSTED BY:
Overall rating: 5.0 out of 5

"Was looking for a nice laptop to surf the web and music. Does real well. only complaint is the keyboard is a little awkward to type and you have to really press hard for it to register. but for the price you can't really complain."

I'm very pleased!

POSTED BY: , Ohio
Overall rating: 5.0 out of 5

"I opted for the L755 with very few extras, since I'm not an "extensive" user. It is much faster than my old one, which was what I wanted. When downloading thru the WiFi connection, it pretty much does it right now! The Windows 7 operating system is OK and didn't take long to get used to. The only complaint is that some of my older program applications won't work on it."

Shorsted laptop

POSTED BY:
Overall rating: 1.0 out of 5

"It only worked for 5 days then went completlety ded"

Great features, great value

POSTED BY: , Springfield, IL
Overall rating: 5.0 out of 5

"The 15.6" display is a nice size for functional desktop use and yet still portable (versus a smaller 14" or larger 17"). The display is sharp. I like the feel of the keyboard and appreciate the numeric keypad. Good sound for laptop speakers. Memory card reader and HDMI output are handy. With 4 GB memory and the Intel i3-2310M processor, performance is great for most users."

A fluke

POSTED BY:
Overall rating: 2.0 out of 5

"I love the combination of higher end hardware at a great price. This is my second Toshiba Satellite. Unfortunately, after a month of use, the hard drive started to fail. Toshiba was good enough to allow Geek Squad to replace the drive on site, saving me weeks of down time. I am still a loyal Toshiba Satellite fan--they pack a lot of value into these machines. I am still recommending Toshibas exclusively, but I fear if I see another machine that fails, that may change. At this point, they are still worth the benefit of the doubt."

1st laptop

POSTED BY: , texas
Overall rating: 4.0 out of 5

"everything works great on the laptop, may note this is a stay at home laptop. little heavy to transport."

Very Nice Laptop

POSTED BY: , ME
Overall rating: 4.0 out of 5

"I would give this computer a 10 rating, as overall i love it. It is much faster than my old Toshiba which i owned for 5 years. My only problem has been two times my computer has frozen up and I've had to turn off the main switch and on again to get is started. This worries me some because it may freeze up sometime and not come back on."

Expected

POSTED BY: , Idaho
Overall rating: 4.0 out of 5

"I love the features,especailly the sticky-notes. they are VERY helpful. However, I don't enjoy the computer spazing out and going to random websites i never even clicked on."

Great Laptop

POSTED BY: , Bandon OR
Overall rating: 5.0 out of 5

"Recently bought this laptop. Tremendous value. Compared to HP at $200.00 higher. Does everything I want. Great screen. Incredibly sharp. Fast. Couldn't be happier"

Great laptop!

POSTED BY: , Denver, Colorado
Overall rating: 4.0 out of 5

"Although I do not use this laptop often enough to enjoy the full features (only use is for school assignments), it so far has performed great for what I use it for. This laptop, however, is very new as it was only purchased about two months ago so I cannot speak on its performance and durability over time. For the time being, the laptop performs great and does not slow me down one bit. It is lightweight and looks great. Even though I have already dropped it, the only result was a small dent near the indicator lights at the bottom due to it crashing into a pole. Durable and looks great!"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.