Toshiba Satellite L755-S5252 Laptop

Satellite L755-S5252

MSRP: $679.99
Satellite L755-S5252 4.33 out of 5.0 based on 6 user reviews. Average Customer Rating: 4.33 out of 5.0
Read Reviews (6) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5252 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5252 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite L755-S5252

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L755-S5252 Laptop Customer Reviews

Good for the price

POSTED BY: , La Paz, Bolivia
Overall rating: 4.0 out of 5

"It is a very good machine for the price, it is a home use computer, you can't do a big and heavy work very well, but is a little slow for that, but it worth the price"

Very Good, Quality laptop

POSTED BY: , Long Island, NY
Overall rating: 5.0 out of 5

"Great laptop overall, I've had no problems, very quick and reliable, screen is great, features are plentiful including the sleep and charge usb and the eco mode gives great battery life. The brushed blue aluminum exterior is a great look. You will not be dissappointed, great value as well."

My best laptop thus far!

POSTED BY: , Costa Mesa, CA
Overall rating: 5.0 out of 5

"I have three Toshiba laptops, one 14", one 17" and this one which is 15.6". All are still working well, and course this new addition works great after setup. I copied the image of the computer to five DVD's. All completed easily. I did not like the fact that no backup disks where supplied. Otherwise I am very pleased with this purchase of a Toshiba Satellite L755. It has plenty of memory and a large hard drive. You will never regret buying Toshiba products!"

Good machine

POSTED BY: , Chile
Overall rating: 5.0 out of 5

"So far I'm very pleased with this machine, good performance, is quite fast and I had no problem so far. In appearance looks nice addition to its aluminum housing that makes it quite robust, as the weight is fairly light in camparison to another computer I have, the screen has good brightness and sharpness. While I am not an expert on computer equipment this machine has left me quite surprised."

POSTED BY: , Irvine, CA
Overall rating: 4.0 out of 5

"Sleek and very fast. No problems what so ever! Great picture! (Last review ^^^^ somethings wrong with ur comp...)"

On Hold

POSTED BY: , Lakewood, NJ
Overall rating: 3.0 out of 5

"It has been freezing up lately despite all the protective software on it - not sure what to do but if I have to send it back and be without a computer for several weeks I will throw it through the window of the retail store and purchase a Mac..."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.