Toshiba Satellite L755-S5306 Laptop

Satellite L755-S5306

MSRP: $531.99
Satellite L755-S5306 4.54 out of 5.0 based on 26 user reviews. Average Customer Rating: 4.54 out of 5.0
Read Reviews (26) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5306 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5306 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor

Satellite L755-S5306 Laptop Customer Reviews

Fast Laptop with Great Features

POSTED BY: , Angleton, TX
Overall rating: 5.0 out of 5

"Fast Laptop with great features. Lightweight, with sleek design. I especially like the 10-key pad on the keyboard, which most laptops don't have."

ok laptop

POSTED BY: , Verona Pa
Overall rating: 3.0 out of 5

"don't like were usb and power ports located my old satellite m35x was better with these things having trouble with this 64 bit set up"

POSTED BY: , Monmouth, OR
Overall rating: 5.0 out of 5

"Great computer. I rated it average on performance because of how the keyboard, pad work. I have trouble getting used to it because the mouse pad is off to the left so I am always missing it. But I'll get used to it. It stopped connecting to my wireless network automatically. I can not find any way to fix it. I was hoping there was a little switch on front like the diagnostic message said to check. Have to go to Fn/F8 to turn off, then back to turn on; then it connects. (my older toshiba satellite still hooks up automatically) can't yet find a manual. And I love the long life battery!! It is a very light and thin computer which is great too. I highly recommend it. (wish someday someone comes out with a key board that lights up!)"

POSTED BY: , canton michigan
Overall rating: 4.0 out of 5

"All seems well so far, I wish the center row of keys had some texture difference because with the number pad(which is new to me) my hands seem off centered and i still make mistakes typing."

POSTED BY: , dalonega, ga
Overall rating: 5.0 out of 5

"This is my first laptop,but I love it. I am still about all the great features."

Good Computer for the price

POSTED BY:
Overall rating: 4.0 out of 5

"The computer does what I need for home use. For the price, it is a great deal. I would not recommend the I-3 processor for heavy graffics."

Great laptop for a good price

POSTED BY: , Boston, MA
Overall rating: 5.0 out of 5

"This laptop meets all my needs as a casual user. It has great speed for the money. Good overall value"

love it love it love it

POSTED BY: , ohio
Overall rating: 5.0 out of 5

"Runs fast, no crashes.....better than a tower."

Nothing Less Than AWESOME!!!

POSTED BY: , Lawrenceville, Il
Overall rating: 5.0 out of 5

"This is my second laptop, I compared several different brands, features, and prices. This Toshiba definitely overruled anything I found. The only thing I wish this laptop had that I found on others is the CD label burner. Other than that, It has everything I need, and probably more."

Excellant for what it cost

POSTED BY: , Ossining
Overall rating: 5.0 out of 5

"Great economical laptop. Battery life with the included battery was good but I needed longer time due to working in the field often so I purchased extended life battery. Picture quality is great as well. Could not be happier."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.