Toshiba Satellite L755-S5349 Laptop

Satellite L755-S5349

MSRP: $579.99
Satellite L755-S5349 3.90 out of 5.0 based on 10 user reviews. Average Customer Rating: 3.90 out of 5.0
Read Reviews (10) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L750s that are available:
Satellite L750 Series »
Laptop Accessories
Shop for Satellite L755-S5349 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L755-S5349 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite L755-S5349

Accessories
Carrying Cases
Batteries
Docking & Expansion

Satellite L755-S5349 Laptop Customer Reviews

toshiba logo

POSTED BY:
Overall rating: 1.0 out of 5

"The toshiba logo is annoying on the web browser. Tried to replace the default browser to Firefox but it would not allow me...keeps opening the one with the Toshiba logo on it... Toshiba seems to be so pushy! Browser is fixed to the Toshiba webpage...this product is not user friendly. Battery is poor...in 2 hours it is dead. Would never buy this brand again."

complete disapointment

POSTED BY: , hart county Ga.
Overall rating: 1.0 out of 5

"I had the laptop less than ten days when it stopped woking"

Excellent laptop!

POSTED BY: , Buena Park, CA
Overall rating: 5.0 out of 5

"I absolutely love this laptop! It is so fast! It is also very easy to use! There is only one drawback and that is the battery life. I keep it plugged in most of the time. I did use it without the adapter and it seemed like the battery went down to 50% after a little over an hour of use."

my favorite laptop

POSTED BY: , Pioche NV
Overall rating: 5.0 out of 5

"ez to operate"

Excellent laptop

POSTED BY: , Atlantic, IA
Overall rating: 5.0 out of 5

"I am very happy with my new Toshiba laptop. It works like I expected and is a nice size to handle. I would highly recomend it to my best friend."

Easy to Use

POSTED BY: , Millersville,PA
Overall rating: 5.0 out of 5

"This laptop is very easy to use and get around. Very easy for a "newbie" like me to use. Would highly recommend this for any "newbie' to learn on."

Not disappointed!

POSTED BY: , Metropolis,IL
Overall rating: 5.0 out of 5

"This laptop is very sleek and light wieght. It boots up very quickly and is very easy to use. And the battery life is great."

Great Tool

POSTED BY: , BEl AIr, MD
Overall rating: 5.0 out of 5

"I have not yet reviewed all the features like file sharing and wireless printing but so far so good. Another USB port would be nice, and moving them to the rear of the case would add another star to features. Having the ports at the front of the machine creates a lot of clutter!"

Tosh5349iba l755-S

POSTED BY: , Northern California
Overall rating: 5.0 out of 5

"Pleasantly surprized with this laptop computer. Not to much bloatware, and what there was, was easy to uninstall. The computer is fast and most of all, it is quiet and lightweight. The fan hardly ever runs. It stays at 40C or less all the time. The screen is excellent. Overall, a great laptop computer."

Problems

POSTED BY: , bradenton, fl
Overall rating: 2.0 out of 5

"Used this machine for less than a month. It frequently shut down on its own and required restart in Windows safe mode. It also made a noise in the DVD player area approximately every half hour as though the player were starting."
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
    Starts at: $890.99
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
    Starts at: $886.99
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
    Starts at: $260.00
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
    Starts at: $389.99
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
  • P50P50
    Satellite® P50
    Optional touchscreen
    Entertainment-focused features
    New-to-market technology
    Premium speakers
    Sleek, elegant styling
    Starts at: $699.99
  • P70P70
    Satellite® P70
    Broad, brilliant viewing
    Entertainment-focused features
    Stunning visuals
    Premium audio
    Perfect desktop replacement
    Starts at: $899.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.