POSTED BY:
PC T3CH
,
VENTURA, CA
Overall rating:
1.0 out of 5
"it was a great computer till the motherboard went out."
POSTED BY:
headache
,
new orleans, LA
Overall rating:
5.0 out of 5
"The laptop performs well, seems to be well built, the software which is installed makes unit perform well; both the Toshiba and Windows 7 installed software. I have received a couple of compliments on the look of the unit which was not necessary but nice to hear for sure. I do not think I have used all of the features installed on the computer but that will come with time and I am sure they will perform like the everything else so far..."