POSTED BY:
Tmac
,
Martinsville, VA
Overall rating:
5.0 out of 5
"Toshiba puts out an excellent product. If investing in a new slimline laptop, you cannot go wrong with this 17.3 size version. Ulta slim, ultra performance."
POSTED BY:
r7russ
,
Lodi, CA
Overall rating:
4.0 out of 5
"This is a great machine with one exception: the keyboard. The keys are perfectly flat and have almost no space between them. It's like trying to touch-type on a cookie sheet. A proper keyboard has sufficient space between the keys to help avoid errors. Even better, make each key a little convex on the surface, which further helps the typist to get it right. This keyboard is a typo generator like none other I've ever used. Aside from that, it's an excellent performer with a brilliant display screen."
POSTED BY:
None
,
Las Vegas, NV
Overall rating:
5.0 out of 5
"I did some research and the Toshiba Satellite was highly recommended. The resolution is spectacular and speed is great. Not crazy about the keyboard, never having a laptop before, so I bought a wireless full size to get me through the transition. Overall, it has been a real pleasure. I'm replacing my dying desktop with this."
POSTED BY:
pete
,
Poulsbo, Wa
Overall rating:
2.0 out of 5
"Performance is inconsistent and slow. Sysfader; a display control function that slows the computer takes over and stalls. Search doesn't show location or access to function. I've thought that I would return the computer if this can't be resolved."
POSTED BY:
"peg"
,
Roseburg,OR
Overall rating:
5.0 out of 5
"In comparrison to the old Dell, this is the "rolls royce" in computers. Thank you Toshiba."
POSTED BY:
Jackel
,
NW, Illinois
Overall rating:
4.0 out of 5
"Thrilled to have a new laptop (desperately needed one). Such an improvement. Great graphics. Easy set-up. Love the keyboard and went with the 17" screen. Not necessary - but glad I did. Pretty much use at the house - not a road warrior."
POSTED BY:
Tiajuana
,
Northern NJ
Overall rating:
5.0 out of 5
"I purchased this laptop for the large screen as my older HP was on it's last legs. So far I have had no issues and highly recommend it. The battery life has been great but I have not had enough experience with it to rank it excellent. If it had Bluetooth, it would be perfect."
POSTED BY:
Countrygirl2of6
,
El Dorado County, CA
Overall rating:
4.0 out of 5
"I miss some of the hardware features of my last Toshiba Satellite - roller wheel to adjust sound, 4 USB ports (new one only has 3! NOT ENOUGH!), missing keyboard keys/rearrangement, etc - there are enough changes to the keyboard that there is a learning curve to familiarize myself with it, but it is a fast, beautiful machine. Love the new screen. Not thrilled with forced change to Windows 7 from XP but that isn't Toshiba. You've done an overall great job with this computer & I will definitely continue to rave about Toshiba over the competitors!"
POSTED BY:
mitzi
,
modesto ca
Overall rating:
4.0 out of 5
"i think i'm going to like having a laptop it takes some getting use to it i like using a mouse better than the pad. but i think i will like it. ti is a lot faster than my old computer."
POSTED BY:
cassie
,
nashville,tn
Overall rating:
5.0 out of 5
"love the screen size, it is great. I needed a new work laptop and it fit the bill."