Toshiba Satellite L775D-S7340 Laptop

Satellite L775D-S7340

MSRP: $649.99
Satellite L775D-S7340 4.40 out of 5.0 based on 78 user reviews. Average Customer Rating: 4.40 out of 5.0
Read Reviews (78) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L770s that are available:
Satellite L770 Series »
Laptop Accessories
Shop for Satellite L775D-S7340 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L775D-S7340 or try our Laptop Forums for additional help.
AMD Vision A6
Accessories for the Satellite L775D-S7340

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L775D-S7340 Laptop Customer Reviews

Awesome computer, but is it too big??

POSTED BY: , PA
Overall rating: 5.0 out of 5

"This computer is AMAZING!!! It is super quiet and super light for a 17+ incher. The only complaint I have is the mere size. It is tough to buy a case for it or a safe to store it in your dorm. I dont understand why all these people are complaining about the keyboard, I like the way that it is set up, you dont have to cross the entire keyboard to type a word which is suprising, so I would say they did a good job setting it up. This computer is fast and has the ability to explore the web with amazing speed as long as your connection is good. However, this computer doesn't have a very sensitive wifi sensor thing cause it usually cant pick up some wifi for whatever reason. But as a computer it is something that im glad I invested in!!!!!!!"

very good laptop

POSTED BY: , ft laud.fl.
Overall rating: 4.0 out of 5

"this is my second toshiba laptop .its better than the other brand that i previously own .i am happy with the battery life its a big improvement from the one i had three years ago."

Spacebar

POSTED BY: , Greer, SC
Overall rating: 1.0 out of 5

"Purchased laptop with numeric keyboard on right side of keyboard. This apparently has thrown everything off. Keyboarding or typing is affected. The spacebar is at least 5/8" shorter resulting in constant errors never happening before - thumb misses hitting spacebar effectively. Cannot type without errors caused by this misalignment. Hate it. Would never buy this type again. Also, the touchpad went out after four months from purchase. Had to send laptop back at my expense. It was repaired within a week and returned to me which was great. But should have been able to send it back COD as it was not my error."

Good Sized laptop gor Movies and Casual Games

POSTED BY:
Overall rating: 5.0 out of 5

""

Stylish but lacking in ease of use

POSTED BY: , Cape Coral, Fl
Overall rating: 3.0 out of 5

"There are several extremely irritating functions that I have not been able to disable. The first and most aggravating is that you cannot lock the screen and its contents at the default 100%. You constantly have to hit hit CTRL + 0 to return things to normal. No matter how vigilant you try to be you will find the screen has magnified on its own to 200, 300 % etc. Sometimes it will go the other way and reduce down to 50,or 25% etc. The second irritation is the wandering cursor..you will often find that you cannot take your eyes off the screen for a second for fear that whatever you are typing will show up somewhere other than where you intended it. The third irritation is the scroll bar on the right side of the screen. I have no clue what makes this change but occasionally a smaller sliding scroll bar will appear and I guess it's supposed to allow you to scroll down thru a lengthy page easier but it really appears to have a mind of its own. Other than that it is a very stylish laptop and has many bells and whistles."

Not the best but that is what I can afford...

POSTED BY: , New York
Overall rating: 3.0 out of 5

"I didn't have a good experience with it at the being and had to get the first one exchanged. The sound stereo makes a wired sound."

Great Laptop

POSTED BY: , Central Utah
Overall rating: 5.0 out of 5

"I shopped and shopped for a new laptop to replace my outdated HP. There are a lot of great laptops out there, and I chose this one because it had everything I wanted at a very affordable price. I have a flight simulator hooked up to it and it exceeds my expectations for visual and sound! I'm very pleased with my final choice."

Amazing Laptop

POSTED BY: , Seminole, FL
Overall rating: 5.0 out of 5

"So i have been using this laptop for a while and I got to say I can play Skyrim with no problem you can even hook up a Xbox controller to it and its a great gaming laptop and great for editing video and if you use Sony Vegas its just amazing recommed you up great the RAM after with free 15% off 2 extra gigs of Ram is toatley worth it."

POSTED BY:
Overall rating: 5.0 out of 5

"I honestly have no complaints about this model and it has actually performed beyond my expectations. I have installed 20 of the top videogames from the past few years and it runs every single one very well."

Great Laptop

POSTED BY: , Cleveland, Ohio
Overall rating: 5.0 out of 5

"So far I am very happy with this laptop."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.