Total Price:
$399.99
*ToshibaDirect Exclusive. Price includes applicable discounts.
**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.
POSTED BY:
Chris
,
Pikeville, KY
Overall rating:
4.0 out of 5
"Love the laptop, but I agree with the other review it's so not built for music, speakers seem to lag and fluctuate way to much! One minute loud next minute muffled, I even adjusted the SRS HD sound and doesn't help even if you turn the SRS off!! But other than that the computer has been good! Fast and all that!!"
POSTED BY:
wifi generation.
,
new zealand
Overall rating:
4.0 out of 5
"Have owned this one for a few months, was an upgrade from an old HP Compaq presario c700, really old Compaq (dual core 1.6, 2G ram) I got the Satellite because it has reasonable specs for a moderate price so i could use it as a gaming/ media computer, however despite it being quick and great with gaming, its been really let down by its sound software/hardware.. that "SRS sound enhancement" they designed to create dynamic realistic premium sound - really only just causes the sound to fluctuate between quiet, and eardrum piercingly loud depending on the tempo of each part of the song currently playing, which just makes you feel physically queasy trying to listen to it.. and further more it really lacks in full sound (all treble no bass) Have even tried disabling SRS and manually adjusting the sound to little effect, just have to search web discussions about the sound quality of these models to know its a widespread opinion of the owners trying to find solutions to the issue. It's a great computer in terms of hardware and capability and so far iv'e never had an issue with gaming performance, but when it comes to sound quality, my old Compaq (which wasn't exactly high spec when new!) is far better for playing music on... how technology has improved over the years!?"
POSTED BY:
Fleet
Overall rating:
2.0 out of 5
"I got this laptop with the A10 processor so I could do some gaming on it. The laptop meets recommended settings but games perform POORLY because of the severely outdated drivers!!! Toshiba will not allow you to install the drivers from AMD and users will have to wait for the Toshiba release the drivers that get updated maybe every 3 years."
POSTED BY:
Lazar
,
Brooklyn, NY
Overall rating:
3.0 out of 5
"Generally L850D-BT2N22 it is a good laptop, but it is missing keyboard backlight-- something I did not realize when I was ordering. A tech support spent 5 minutes tryng to figure out if this model has backlight. I had to install a table lamp, without which it was difficult to use the keyboard."