Toshiba Satellite L855D-S5220 Laptop

Satellite L855D-S5220

MSRP: $548.99
Satellite L855D-S5220 4.35 out of 5.0 based on 23 user reviews. Average Customer Rating: 4.35 out of 5.0
Read Reviews (23) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L850s that are available:
Satellite L850 Series »
Laptop Accessories
Shop for Satellite L855D-S5220 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L855D-S5220 or try our Laptop Forums for additional help.
AMD Vision A8
Customize your L850 at ToshibaDirect.com

Customize

Accessories for the Satellite L855D-S5220

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite L855D-S5220 Laptop Customer Reviews

I love my Laptop!

POSTED BY: , Delco, NC
Overall rating: 5.0 out of 5

"My husband got my new Toshiba for me and I love it. It's fast and efficient. I love the battery life. I can work on it for hours before I have to plug it back in. I will always buy Toshiba!"

Toshiba is Number one

POSTED BY: , Davenport, Iowa
Overall rating: 5.0 out of 5

"I read a lot about laptops before my purchase. I rely a lot on Consumer digest. You are rated number 1. After receiving my laptop I now know why. This is the best!! Thank you."

LOVE MY TOSHIBA

POSTED BY: , DUBOIS, WY
Overall rating: 5.0 out of 5

"I replaced a Toshiba laptop that I purchased in 2007. The hard drive capacity in the old computer was small compared to this and the battery life was minimal. This one lasts 6 hours, awesome! Also great display and processor. Love everything about it!!"

Great Laptop

POSTED BY: , Sacramento,CA
Overall rating: 5.0 out of 5

"Downloads super fast, clean clear picture, and easy to set up."

Excellent!

POSTED BY: , Tampa, FL
Overall rating: 4.0 out of 5

"Even though I have heard the battery life is not that long, I have to say I'm extremely happy with the one of this laptop. It averages 2-3 hours, which I believe is great. Of course, this also depends on the programs you are running on the machine. Regarding the sound quality issues, the SRS Premium Sound Software that comes pre-installed pretty much solves the whole problem, which takes out almost all the drawbacks of this laptop. The only reason I'm not rating it 5 stars is the layout of the keyboard, specifically the design of the "F-number keys," as I would prefer to hit F5 or F1 by themselves instead of having to press FN and then F5 or else I would deactivate the touch pad. Other than that, this laptop is, in one word, excellent. Recommended!"

GREAT LAPTOP FOR PRICE!

POSTED BY: , SARATOGA SPRINGS NY
Overall rating: 5.0 out of 5

"ONLY issues are the battery life & the speakers...would buy another in a heartbeat!!!"

excellent laptop

POSTED BY: , killbuck, ny
Overall rating: 5.0 out of 5

"I would highly recommend this laptop to anyone. I love the keyboard and I love the picture quality. I do wish the keyboard was lit up a little."

The Best

POSTED BY: , Illinois
Overall rating: 5.0 out of 5

"This Toshiba laptop is my first laptop but I,ve come to realize in the short time I've had it that I would recommend it to anyone. I am completely satisfied."

Love this Laptop

POSTED BY: , Point Pleasant, NJ
Overall rating: 5.0 out of 5

"The screen is an execellent size and with 6 meg of memory everything loads down so fast. Having 650 meg of storage space is huge plus. I find surfing the net and loading down files an ease. Highly recommend this product."

Toshiba Laptops

POSTED BY: , Pittsburgh, PA
Overall rating: 4.0 out of 5

"I keep buying Toshiba Laptops cause they have lasted longer than other brands. I use it pluged in most of the time and the A/C adapter plug is a solid conection. Other brands are loose and break too easy."
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
  • L850
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.