Toshiba Satellite L875D-S7230 Laptop

Satellite L875D-S7230

MSRP: $579.99
Satellite L875D-S7230 3.71 out of 5.0 based on 14 user reviews. Average Customer Rating: 3.71 out of 5.0
Read Reviews (14) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite L870s that are available:
Satellite L870 Series »
Laptop Accessories
Shop for Satellite L875D-S7230 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite L875D-S7230 or try our Laptop Forums for additional help.
AMD Vision A6
Customize your L870 at ToshibaDirect.com

Customize

Accessories for the Satellite L875D-S7230

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite L870 Series Laptops
L870
Model: MSRP:
L875-S7108 $531.99
L875D-S7332 $549.99
L875D-S7131NR $604.99
L875D-S7342 $629.99
L870D-ST4NX1 $529.99*
L875-S7153 $699.99
L870-ST4NX1 $549.99*
L870-ST4NX3 $829.99*
L870-ST4NX2 $729.99*
L875-S7377 $999.99
L870-BT3N22 $479.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite L875D-S7230 Laptop Customer Reviews

Not bad!

POSTED BY: , North, AK
Overall rating: 5.0 out of 5

"Not exactly what I was looking for when I went shopping for a laptop, but it is serving its purpose very nicely. My choice was driven solely by the operating system, I hate Windows 8. This is my second Toshiba laptop, a major improvement over the first. This one is much faster and more stable. It wasn't bogged down with all the junkware the 1st had either, making it quick to set up and go. The 6 gig ram is okay, but make use of its 16 gig max ram, it really woke things up."

BEST LAPTOP TO BUY

POSTED BY: , GREEEN BAY WI
Overall rating: 5.0 out of 5

"THIS IS THE THIRD TOSHIBA LAPTOP WE'VE HAD.. THE FIRST ONE WAS ABOUT FIVE(5) YEARS OLD WHEN WE GOT OUR PRESENT ONE.WE HAVE BEEN VERY SATISSFIED WITHN IT AND WOULD RECOMMEND TOSHIBA TO ANYONE."

Works Great with Windows 7

POSTED BY: , Pittsburgh
Overall rating: 4.0 out of 5

"I bought this about 5 weeks ago. I had no complaints with how it came out of the box with Windows 7. Worked flawlessly. Very Happy. Then I fell for the upgrade to Windows 8. Complete nightmare that I am working on for day #3...It began with a partial loss of my keyboard functions....now I have no Wi-Fi. If you are going to buy this and want 8...buy it with 8 installed. If you wish to upgrade to 8...BEWARE....and back everything up twice.....then take some time off work so you can try and get 8 to work right."

Not What I Expected

POSTED BY: , Honolulu, HI
Overall rating: 2.0 out of 5

"For the money the Toshida Satellite L875D-7230 Laptop was okay...but would not purchase again...I needed to return the laptop twice to the store before I was satisfied with it's performance"

My New Laptop

POSTED BY: , grand ra[ids mi
Overall rating: 4.0 out of 5

"I only had one other laptop for comparison. I like the big screen. I went online to read the directions for use. They were not very specific. I was going to print them for use as a reference guide but they did not contain any information on how to do things or short cuts that I am not aware of but are available for more knowledgeable users. Maybe that is a seperate book I'm not aware of. Information of that type should be included with a purchase. It would be handy. I find this laptop difficult to open otherwise it is similar to others. I haven't had it long enough to havve much other info for you..."

One for the money

POSTED BY: , Bemidji, Mn
Overall rating: 4.0 out of 5

"This 17 inch laptop replaced a similar unit that was 7 years old, so the speed is much better. The display also seems crisper and it fires up much faster. Without being paranoid about it, I have yet to get a low battery warning. These are important valuable features. The touch pad is quirky compared to my earlier one and I haven't figured out how to reconfigure it so it doesn't change scale everytime I try to drag something. It also keeps telling me that internet has stopped working and it won't open facebook pictures except by starting with a blank that I have to advance from and then back up to see the first image. Maybe that is software, maybe hardware. I'll try to figure that out too. Overall, for the price it is grand, but awkward during the breakin period."

Good Value

POSTED BY: , Idaho
Overall rating: 4.0 out of 5

"Very nice laptop. Make your first upgrade to a total of 8 GB. I bought it as my 4th Toshiba 17 inch laptop expecting to add a second drive to the machine (SSD Boot Drive). No interface for a second drive on this model. I wish I would have known that before purchase since the other Toshiba laptops had slots for 2 HD's."

Sounds good, looks great!

POSTED BY: , Petersburg, Ohio
Overall rating: 5.0 out of 5

"I'm new to computers, but I like my laptop. I like the big 17 inch screen and theToshiba Health monitor is very helpful. It set itself up real easy, and the sound quality is much better than others I've heard. I looks sleek. Overall, very happy."

First time to use a laptop so it takes some

POSTED BY: , Minneapolis, MN
Overall rating: 4.0 out of 5

"getting used to."

Can't imagine needing anything more!

POSTED BY: , Tempe, AZ
Overall rating: 5.0 out of 5

"It has plenty of speed and hard drive capacity. I have lots of pictures and it is not even close to full. It has great battery life (usually over 4 hours). A minor negative is the mute button takes 2 seconds to respond to turn sound either on or off."
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
  • L870
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.