POSTED BY:
Bobby88
,
FL
Overall rating:
3.0 out of 5
"This is my third Toshiba. Will be my last. Product feels average. Not particularly fast. the HK speakers are just OK. one key of the keyboard is already crooked (less than 1 month of light use). HD is too sensitive to movement. and W7 tracks my surfing like crazy. never had so many targeted ads when surfing the net."
POSTED BY:
esalg420
,
Miramar, FL
Overall rating:
4.0 out of 5
"I have to say I had high expectations for this computer which may be why I have been somewhat disappointed with it. My main complaint with it is the WI-FI which takes atleast a 60-90 secs to connect to a signal every time the computer wakes up from sleep mode. Also the range on it is limited in comparison to other computers as it usually needs 4-5 bars just to connect, rarely will it connect with 3 bars and anything below that you can forget about it. Also the "illumination" button is a useless feature for this computer as it is meant for models with a back-lit keyboard. This model is not back-lit no matter what the specs say so don't purchase it expecting the back-light for the keyboard. As for positives it has an above average battery life and runs pretty quietly. For the price it is definitely worth a look but the cons might be annoying enough to look at another model."