POSTED BY:
Jake
,
United States, MO
Overall rating:
4.0 out of 5
"This is a great device with many great specks and features. The main problems I found is a average battery life, a poor graphics card, and even though it has a core i5 processor programs and mostly the internet run very slowly."
POSTED BY:
Bear
,
OHIO
Overall rating:
4.0 out of 5
"Feature and performance wise been very happy with it. use it when traveling. Love the built in webcam and media reader. The Bluray drive is an added bonus that I've used for watching movies My only negative is the battery which has slowly failed to the point I'm getting a constant suggestion to replace the battery"
POSTED BY:
Rick
,
San Diego, CA
Overall rating:
3.0 out of 5
"I have had Toshiba in the past and have liked it. Sound is better than the Dells we have at home. Though, on this model the keyboard takes extra effort on each key than an average laptop, so get ready for your fingers' workout. It said 7 hours battery life when I purchased it, but it barely gets to 1.5. So I guess it is the same story as the EPA mileage on cars, all unreal data. Also, the touchpad is quite sensible and has made me accidentally move folders into other folders in 2 steps: a) open a folder and move around to try to open a sub-folder. The touchpad is weird, as compared to the other laptops at home. It thought it was only me, but my family members commented the same."
POSTED BY:
Haryokanmey
,
Ilorin, Nigeria
Overall rating:
4.0 out of 5
"i got this laptop from US sometime around August and I actually got it open Sept 6, After charging and checking the PC Health Monitor, i discovered my battery is "Fair" and after two weeks, It degraded to poor which doesnt last more than 2hrs 30mins at "Poor" stage. I think the battery is bad from the factory because I discovered it has been plugged into my system instead of separating it as they did to Charger otherwise its a great system......My friends tagged it MACHINE."
POSTED BY:
TheQueen
,
springfield mo
Overall rating:
5.0 out of 5
"ive only had toshiba laptops. this one i really like. blu ray is awsome its really fast. everyones loves the style of it. it does everything and plays my games sweet. love it"
POSTED BY:
Krazyleft
,
broward county, fl
Overall rating:
1.0 out of 5
"all toshiba products have all the hardware that is up to date problem is alot of the laptops have power supply problems or shorts within the motherboard , this is my second toshiba sat. and i had to recently send my laptop in once again due to the computer losing power for no reason and shutting down totally ."
POSTED BY:
MzFinney
,
springfield mo
Overall rating:
5.0 out of 5
"this laptop does everything i need and want it to. 14" is nice. love the widescreen. im on it all the time and the battery stays pretty good. for the money, you wont beat this cool laptop. blueray is very cool. first time watching movies with it, very clear"
POSTED BY:
Tony
,
Union City, IN.
Overall rating:
5.0 out of 5
"this is my first laptop ,I have played around on some . I did not know if I wanted a14" or a15.6". I chose the 14". So how do I like it, well I think it is a great laptop , I like the size of it, it's not that heavy, it's a compact laptop. Good job done TOSHIBA. But I think you should have a little bigger battery, for the price of the outfit or you can add a AC Mobile Power Inverter, so you can run or charge your laptop from your car."
POSTED BY:
Corsario
,
Brasil - Brasília
Overall rating:
4.0 out of 5
"It has a very good performance and price but deserves a better resolution display and a metal case."
POSTED BY:
John
,
Phoenix, AZ
Overall rating:
3.0 out of 5
"Like the bluray, plenty of ram and hdd space. Lacking enough video memory, struggles to play dvd's and bluray, widi is limited also."