POSTED BY:
Nance
,
Florida
Overall rating:
3.0 out of 5
"I really like my Toshiba Satelite P750-ST4N01 Laptop, but I do not like Windows 7 at all! I truly did not know there would be such a difference between Windows 7 and Windows XP which I really loved. Windows XP was so much easier to understand and operate when you are not tech savvy."
POSTED BY:
grammy
,
MD
Overall rating:
5.0 out of 5
"this was a super priced item. It shipped in no time, it works great and I would recommend this laptop to anyone that is looking to buy one."
POSTED BY:
laptop girl
,
Columbus, OH
Overall rating:
5.0 out of 5
"I love my new laptop! It has great features and I have seen similarly priced laptops with much less memory and features. The keyboard is awesome. I am new to laptops so I have had a few challenges with the mousepad and the sensitivity of it and the fact that it enlarges and changes the view of the screen with minimal movement but other than that, it's great!!"
POSTED BY:
SuLung Dragon
,
NYC
Overall rating:
5.0 out of 5
"Very nice laptop, great features irregardless of price. Backlit keyboard was the major attraction for my aging eyes, very fast operating speed was a bonus! Comfortable keyboard and tactile response. Screen is bright and sharp. Harman Kardon speakers are very good for a laptop. Feels pretty sturdy and durable overall. Getting 5 hrs regularly when just surfing which is the primary purpose for this machine. 3 USB 2.0 are standard ot this price, this one also has a USB 3.0 too! Great for external drive backup. I'd buy another if I needed one."
POSTED BY:
DD
,
South Padre Island, TX
Overall rating:
5.0 out of 5
"Sleek, sexy, powerful & full of speed! Love it!!!!"
POSTED BY:
Smoky
,
Green Lane, PA
Overall rating:
5.0 out of 5
"Love the Satellite P750 overall... The only drawback - which may disappear as I adjust to it - is that the mouse pad doesn't always sense my hand-movement, and I have to re-do actions to move the cursor. Love the location of the photo-card slot... the number pad and the lighted keyboard. Battery life has been less than stellar."
POSTED BY:
V...
,
Boston, MA
Overall rating:
5.0 out of 5
"This is a great laptop, great design, pretty satisfied with the performance though I have to say that I upgrated it to an i5 processor. sounds system is excellent."
POSTED BY:
Teeners
,
Plattsburgh, NY
Overall rating:
5.0 out of 5
"I like this laptop very much especially the keyboard. It has back lighting plus the way the keys feel is like butter. This has proven to be a very good computer for streaming video online. One of the reasons I picked this particular model was because of the harman/kardon speakers which are great. I would recommend this model to anyone that wants a good computer for streaming online as well as for playing games online."