Toshiba Satellite P750-ST6GX2 Laptop

Satellite P750-ST6GX2

MSRP: $1,199.99
Satellite P750-ST6GX2 4.54 out of 5.0 based on 13 user reviews. Average Customer Rating: 4.54 out of 5.0
Read Reviews (13) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite P750s that are available:
Satellite P750 Series »
Laptop Accessories
Shop for Satellite P750-ST6GX2 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite P750-ST6GX2 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Satellite P750-ST6GX2

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite P750 Series Laptops
P750
Model: MSRP:
P755D-S5266 $749.99
P755-S5383 $774.99

Satellite P750-ST6GX2 Laptop Customer Reviews

Fast Lap!!

POSTED BY: , Jacksonville, Fl
Overall rating: 5.0 out of 5

"Use this lap on avg about 50 hrs a week with no problems so far. Upgraded to Samsung 830 256 SSD, Corsair 16GB Ram and W7 Pro 64-bit and now boots up in 12 secs flat! Like the backlit keyboard which you can set in bios. Only minor knock would be the dvd tray door hanging up on the power cord,, Toshiba needs to move the power plug to opposite side and then problem would be solved."

POSTED BY: , Mongolia
Overall rating: 5.0 out of 5

"Hello! I'm from Mongolia. It's the Best Laptop Ever I have. It's my first laptop:) I'm very HAPPY!! whit it.:D"

Haven't used long enough

POSTED BY: , Chandler, AZ
Overall rating: 3.0 out of 5

"I just recieved the lap top and haven't used it enough to give an honest opinion on the lap top it self. My experience with Toshiba Direct was not very good. I am not sure I would use them again."

Toshiba Fan

POSTED BY: , Chicago Suburbs, IL
Overall rating: 4.0 out of 5

"I'm generally pretty happy with this laptop. It is the second Toshiba laptop I've owned. The first bit the dust after 5 years and I tried replacing it with a cheaper brand floor model. After a year of frustration I gave that piece of junk to my son and bought another Toshiba. I love the backlit keyboard...it is great to use when watching tv. Since I often type with the laptop on my lap, I'm finding that the buttons below the keypad are a bit oddly placed; they are way-far forward and I'm having a difficult time getting used to them. The features are great (as expected) and so is the speed...things download very quickly. My battery has been lasting about 3 hours, which is less than I'd like but about what I'd expected, given previous reviews. All in all, I'm very pleased and will continue to purchase Toshiba products in the future.."

Satellite P750-ST6GX2 Laptop

POSTED BY: , TN
Overall rating: 5.0 out of 5

"Excellent computer, very fast, easy to use and like the back light on the keyboard"

good lap but low battery life

POSTED BY:
Overall rating: 4.0 out of 5

"over all lap was worthy but battery life low battery charging down with in 2-3 h even i put eco mode (low power use age).. remaining all features are good.I taken Toshiba lap for long battery but I didn't satisfy."

awesome laptop

POSTED BY: , Kennebunk, ME
Overall rating: 5.0 out of 5

"The speakers on this lap top are great. I very seldom have to turn them up past 30. The battery life, once calibrated last 2 to 3 hours. I bought the 12 cell winch lasts upwards of 6 hours. The screen is bright and the colors vibrant. The back-lit keys are great!!"

Powerful laptop with nice features

POSTED BY: , Santiago, Chile
Overall rating: 5.0 out of 5

"Purchased this model mainly due to its fast processor and large amount of RAM, as I do a lot of financial numerical analysis, which requires powerful computers. So far I'm happy with the speed at which my programs run, and I can't complain about the added goodies, including the bright screen and great graphics, responsive keyboard, and large HD. Unless I'm doing something wrong with it, I think the bundled webcam is inferior to most other brands today, but that is not a major concern to me."

Nice laptop

POSTED BY: , New Orleans
Overall rating: 4.0 out of 5

"The unit was purchased to replace a desk top computer. To that demanding end, I find it serviceable and adequate. Any complaints I have with the machine is actually with Toshiba direct. The unit was put on sale by a national retailer for 20% less than the "Direct" sale price, moments after I installed my software.... Nice machine though."

Great lapton

POSTED BY: , Iowa
Overall rating: 5.0 out of 5

"This laptop is efficient and provides an array of possiblities for being so compact. The laptop is sleek and has been very reliable."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.