Toshiba Satellite P755-3DV20 Laptop

Satellite P755-3DV20

MSRP: $1,199.99
Satellite P755-3DV20 4.57 out of 5.0 based on 7 user reviews. Average Customer Rating: 4.57 out of 5.0
Read Reviews (7) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite P750s that are available:
Satellite P750 Series »
Laptop Accessories
Shop for Satellite P755-3DV20 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite P755-3DV20 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite P755-3DV20

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite P750 Series Laptops
P750
Model: MSRP:
P755D-S5266 $749.99
P755-S5383 $774.99

Satellite P755-3DV20 Laptop Customer Reviews

Excellent Laptop

POSTED BY: , philippines
Overall rating: 5.0 out of 5

"The features are great, but can you please help me with regards the 3D effects on movies? 3D on pictures and games are great but in movies, i am having a hard time to view movies in 3D, it says .mp4 files or mpeg2, and whenever i use dvd's somethings wrong with the conversion. but this thing is superb :)"

I'm happ with it

POSTED BY:
Overall rating: 5.0 out of 5

"This laptop runs games well even high performance games speed is good. No lagging in the games when in 3D mode. movies good in 3d"

Whatever...

POSTED BY: , Sherveport, La
Overall rating: 3.0 out of 5

"Ummm...yea.. I think this is a really cool laptop and the fact that it is able to play movies in 3D is cool and all...but when i try to play my movies in 3D it doesnt work...the screen splits in two so its like i have two seperate screens that are playing the same thing...and it bothers me that i bought this and the 3D effects arent working correctly..."

I Love Toshiba

POSTED BY: , Malaysia
Overall rating: 5.0 out of 5

"I Like Toshiba. This is the one of the best laptop I ever had.My only complain is that TOSHIBA logo on the laptop is way too big. From 5 meter can see. Honestly It's ugly. Anyway It's doesn't bother me because It will sit on my desk anyway. I have my iPad to carry around with me. I love graphic designing so I get that model. 3D is bonus for me. plus 3D glasses. and"

Excellent Laptop but too many uneccessary toshiba

POSTED BY: , Gardiner, Maine
Overall rating: 4.0 out of 5

"Everything on this Laptop works very well I have had no problems and love the speed and hardware features. the only complaint i have is the excessive number of toshiba apps on this laptop when I got it. I would prefer that the optional programs come as just that, optional with a link to install or a cd if I choose to install it."

Best Laptop Ever!

POSTED BY: , Dominican Republic
Overall rating: 5.0 out of 5

"Toshiba is complete in technology. It meets my needs, all you seek, find it on Toshiba TV, DVD, BLUE RAY, CAMERAS AND ALL ACCESSORIES"

wow

POSTED BY: , Kenya
Overall rating: 5.0 out of 5

"This one of the best toshiba laptops I have seen,I prefer buying it because I like Toshiba"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.