Toshiba Satellite P755-S5215 Laptop

Satellite P755-S5215

MSRP: $722.99
Satellite P755-S5215 4.34 out of 5.0 based on 65 user reviews. Average Customer Rating: 4.34 out of 5.0
Read Reviews (65) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite P750s that are available:
Satellite P750 Series »
Laptop Accessories
Shop for Satellite P755-S5215 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite P755-S5215 or try our Laptop Forums for additional help.
Intel® Core™ i3 Processor
Accessories for the Satellite P755-S5215

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite P750 Series Laptops
P750
Model: MSRP:
P755D-S5266 $749.99
P755-S5383 $774.99

Satellite P755-S5215 Laptop Customer Reviews

Satellite P755-S5215 Laptop

POSTED BY: , Louisville, KY
Overall rating: 4.0 out of 5

"The laptop is sleek, comfortable and the graphics are incredible. The only thing I would have done differently would have been the processor. If I had been paying better attention, I would have purchased a faster processor than the I3. Even with that, it's a great laptop, and I'm very pleased with the product.."

Toshiba Satelite - Worth every penny!

POSTED BY: , Weston, FL
Overall rating: 4.0 out of 5

"I purchased this laptop for work purposes and thus far I am impressed with it's ability and performance. A great buy for the money!"

Best Christmas Present Ever!

POSTED BY: , Grand Rapids, OH
Overall rating: 5.0 out of 5

"Well made product, great video & sound clarity. Love having a full sized keyboard and screen, those net books & tablets are not comfortable for me to use."

Good laptop, except for keyboard.

POSTED BY: , Marion, IL
Overall rating: 4.0 out of 5

"I am going to write this review without editing. I'm a ver good typist... Everything about this computer has been good except for one thing. the keyboard. The sace bar doesn't take a lot of the time as well as other keys on the keyboard. the shift key is another issue as you can seeI've already had 2 words that it didn't take on. It's really frustrated others when they've used it. I don't want to sed it back and wait 2weeks for it to get fixed. Besides that, it's great. much better than the HP's that i've had in thepast."

Excellent laptop

POSTED BY: , Broomfield, CO
Overall rating: 5.0 out of 5

"Works well, responsive and great value. Excellent customer support so far, too!"

Not bad for the cash

POSTED BY: , Venice,FL
Overall rating: 4.0 out of 5

"Yes, you can buy better comps for more money. But dollar for dollar, you can't go wrong with this laptop."

First Laptop

POSTED BY: , Grand Rapids, MI
Overall rating: 5.0 out of 5

"Bought it for college. I have NO complaints! I love it! It's my first laptop ever and I don't regret buying a Toshiba. It's a core i3 but it is excellent! I use my laptop everyday and all day long. No problems :) had it for about 4 months now. Defiantly a great computer."

Best laptop

POSTED BY: , Riverdale, GA
Overall rating: 5.0 out of 5

"I love Toshiba, I have had a HP and I will never go back to one. This is my second Toshiba, my first got stolen and I love it. Keep up the good work. My only complaint is that the battery life is so short."

P755-S5215 works great

POSTED BY: , Salt Lake UT
Overall rating: 5.0 out of 5

"going from a HP to a Toshiba was like going from the stone age to shooting men to mars. i was impressed to find out how reliable this laptop really is (been dropped 4 or 5 times). it's really easy to use, the sound quality is great, the clear picture and the many features and options it gives are also nice. i only have 4 complaints: key's some times stick but very rare. for some reason about once every 2 weeks my volume controls randomly stop working and i have to go in and manually turn them up or down. (not a big problem). also, if there is an option to turn off the power button's light it gives off, i haven't found it but i do find it kind of annoying with it glowing all the time. after the 3 or 4 months of owning it, i've only experienced 1 glitch which sadly ended up in me having to restart the laptop. however, everything i was working on (word, websites) were saved. no other problems have come up other than those. above all: a great laptop with great features, picture and sound. as a Soldier on deployment, a tough, reliable, light weight, and portable laptop are a must. this laptop exceeds all of those. Well done Toshiba!"

Love This Laptop!

POSTED BY:
Overall rating: 5.0 out of 5

"Love the looks and also how fast it runs! Great laptop"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.