Toshiba Satellite P755-S5262 Laptop

Satellite P755-S5262

MSRP: $899.99
Satellite P755-S5262 4.62 out of 5.0 based on 8 user reviews. Average Customer Rating: 4.62 out of 5.0
Read Reviews (8) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite P750s that are available:
Satellite P750 Series »
Laptop Accessories
Shop for Satellite P755-S5262 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite P755-S5262 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
Accessories for the Satellite P755-S5262

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite P750 Series Laptops
P750
Model: MSRP:
P755D-S5266 $749.99
P755-S5383 $774.99

Satellite P755-S5262 Laptop Customer Reviews

Great Value

POSTED BY: , northern IL
Overall rating: 4.0 out of 5

"I think this was an excellent laptop for the price. I'm very happy with overall performance. It took me a little while to get used to the keyboard being off-center to accommodate the number pad, but I'm happy with my purchase. Battery life is OK right now, but I'm afraid that as it ages, it will be an issue. Still, I'm happy with my Toshiba. I'd buy another one..."

Excellent laptop

POSTED BY: , Erie, PA
Overall rating: 5.0 out of 5

"This laptop exceeded all my expectations. It was very easy to set up, the wifi found my router right away and I was on the internet in a matter of minutes. The speed is phenominal. I love it."

A Good Value Laptop

POSTED BY: , PA
Overall rating: 4.0 out of 5

"I purchased this to replace my 4 year old laptop. I love the WiDi capability and it is very fast. I would have preferred better graphics capability but even without an integrated graphics card, it is very good."

Awesome laptop

POSTED BY: , Chicago,IL
Overall rating: 5.0 out of 5

"I got this laptop a little concerned about the price. However, it has turned out to be well worth it in the end. I would highly recommend this laptop to others, and hope they enjoy it as much as i do."

Best Value and Performance

POSTED BY: , Charlotte, NC
Overall rating: 5.0 out of 5

"I have used Toshiba laptops as company provided hardware in past. This is the 1st personal Toshiba I have owned, as former personal laptops were very troublesme. I would only buy Toshiba laptops for personal use and was very happy when the i& technology was released"

Great laptop and customer service

POSTED BY: , Providence, RI
Overall rating: 5.0 out of 5

"This laptop is amazing. I had trouble setting up my internet connection to this laptop and the Customer Service team did a great job of helping me out in a short amount of time. Needed to delete and reinstall new drivers. Great laptop. I have a Toshiba netbook too and love it as well."

POSTED BY: , SPRING,TX
Overall rating: 4.0 out of 5

"GOOD COMPUTER FOR THE MONEY"

Dependable and Reasonable

POSTED BY: , Plano, TX
Overall rating: 5.0 out of 5

"Toshiba is know for its good quality and durable laptops. I use to have Toshiba Satellite but later switched to Sony. I found out the Sony computers are expensive and they break often. Recalling that I never had problems with my Toshiba laptop, I bought a Toshiba this time around. The only negative comment about this P755-S5262 is that there is no integrated Wireless-N receiver installed. A surprising fact!"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.