POSTED BY:
ToGDC
Overall rating:
4.0 out of 5
"Everything seems to work well. I travel a lot - the size and weight of this model is perfect for me. I recommend that you create your rescue media right away on recepit. Along with any downloaded programs. I had to (still not sure why) rebuild my system about three weeks after receipt -- it just would not start. I would also like to see LESS pre-loaded programs, especially Norton products. I use Kaspersky. You cannot load another anti-virus unless you get Norton off. I can only say that is like trying to get a stubborn virus off. The Norton removal tool did not work either. I had to resort to getting into the registry (which is not recommended for most users) to get rid of Norton."
POSTED BY:
DarilynSue
,
United States
Overall rating:
5.0 out of 5
"My new Toshiba laptop is definitely one of the best laptops I've ever owned. The i7 core processor speed is extremely fast, especially when combined with the new Rockmelt browser. I love the wood grain feel & look, which leaves no fingerprints. The design & durability are wonderful. I really love the option to toggle the mouse pad off & on. This helps me so much when I'm typing, as on my past Toshiba Satellite I was always dragging my hand across the mouse pad & it was very frustrating. The speakers are well above par in comparison to other laptops. They’re very loud, not that crackerbox sound. The option to have the keys backlit is kind of nice; however, it does drain your battery a lot quicker. The battery life is not the best on this laptop. I’ve never gotten more than about 2 hours & 45 minutes out of my fully charged battery. I love the voice integration & I love having a keypad on my laptop & the feel & size of the keyboard is very user friendly. The graphics are top notch on this laptop. I’m very pleased with my Toshiba Satellite P755-S5269 purchase & would highly recommend this laptop!"
POSTED BY:
zben123
,
staten island
Overall rating:
3.0 out of 5
"the labtop is quite pricey and the battery life is horrible"
POSTED BY:
KaTT
Overall rating:
4.0 out of 5
"This is my first laptop and I wanted to have it all. The screen quality is mind blowing as well as the sound. It's probably the best speakers on a laptop period. The only thing I'm not so crazy about is the battery lasts only 2.5 hours with eco mode on. Without it it's not even an hour. I wonder if it's just this laptop or is that how all of them are or maybe I'm doing something wrong because it should be 5 hours. The space bar is a little annoying at times because you have to really hit it hard so a lot of times I have to backspace and re-space. Also the touch pad is so-so. The important stuff is what's inside! The speakers alone make up for all the little problems like battery and space bar and touch pad. It's a very impressive laptop and durable."
POSTED BY:
Guido
,
Ohio
Overall rating:
5.0 out of 5
"Thus far, I'm totally impressed with this laptop! This is my first laptop and I couldn't be happier with the features on my P755!! Lightning fast and lots of user friendly features."