Toshiba Satellite P755-S5274 Laptop

Satellite P755-S5274

MSRP: $733.99
Satellite P755-S5274 4.50 out of 5.0 based on 4 user reviews. Average Customer Rating: 4.50 out of 5.0
Read Reviews (4) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite P750s that are available:
Satellite P750 Series »
Laptop Accessories
Shop for Satellite P755-S5274 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite P755-S5274 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite P755-S5274

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite P750 Series Laptops
P750
Model: MSRP:
P755D-S5266 $749.99
P755-S5383 $774.99

Satellite P755-S5274 Laptop Customer Reviews

Toshiba Satellite...Bang for the Buck!

POSTED BY:
Overall rating: 5.0 out of 5

"Need a good, reliable Laptop and funds are low? Consider the Toshiba Satellite....it is a bargain and has all the necessary features."

Good performance for the price

POSTED BY: , harrisburg pa
Overall rating: 4.0 out of 5

"The computer has met or exceeded my expectations. It started and set up easily and works faster than I thought it would. However the battery life could be better and the web cam is not good. I wanted the web cam for Skyping but I will use an external one because it is so bad."

Happy

POSTED BY: , Hattiesburg, MS
Overall rating: 5.0 out of 5

"So far I am pleased with the performance of this product. I am finding the certain keys "stiff" and hope I will learn to compensate quickly."

Good laptop... mostly

POSTED BY: , PA
Overall rating: 4.0 out of 5

"I really like the laptop I got. It runs pretty quickly, however there are a lot of extra programs Toshiba puts on that I've been working to remove as I don't need them. I plan to use this for DJing, but haven't been able to get it to work yet, however the current issue is more with the program/external sound card then it is the laptop."
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.