POSTED BY:
dino
,
Fort Mohave, AZ.
Overall rating:
5.0 out of 5
"every things great! I'm just now getting introduced to windows 7 from XP. Very Nice! WOW!!!"
POSTED BY:
Toshiba Laptop
,
MN
Overall rating:
4.0 out of 5
"I have been using this computer for about 3 months and it's a pretty nice computer. I love the lighted keyboard! I have the i5 processor and it is crazy fast and I didn't think my other laptop was all that bad. The is my first laptop with the number pad so I'm still getting used to the keyboard being off center, but that will come with time. The resolution and image quality is very good. Overall, I'm very happy with this computer and would recommend it to anyone. The battery life can be disappointing, but if you take the time to set the power settings, you can triple the battery length. I'm getting 5-6 hours with adjusted power settings."
POSTED BY:
LeeLee
,
Solon, OH
Overall rating:
5.0 out of 5
"I've used a number of desktiops & four laptops. But let me tell you that this is the best by far! From the start-up, which was the easiest I've ever encountered, to using it for everyday purposes, ie social networking, emailing, writing & saving documents and pictures the Satellite P755-S5381 is excellent. Whether you are new to laptops or an expert, this is THE laptop to get! I highly recommend it."
POSTED BY:
tt
Overall rating:
4.0 out of 5
"This laptop is fast and user friendly"
POSTED BY:
Busy Bee
,
Delaware, Ohio
Overall rating:
5.0 out of 5
"So far - so good. I rated the battery life at a 4 because I have not had an "over extended" use with the laptop yet. This being month one of ownership - I am very happy with this laptop. Comptetively priced - and a lot for my money. I would highly recommend the Satellite P755-S4381 Laptop."
POSTED BY:
Anchor
,
Grand Rapids MI
Overall rating:
4.0 out of 5
"So far, so good. Only issue is cursor magically changes position while typing. Have heard from other Toshiba users that same issue has occurred for them too. Sound quality is marginal. Thought Harmon Karden speakers would sound better. Bought docking station which is really nice extra for multiple devices. Battery seems to discharge faster than I expected. Overall a good value for the money."
POSTED BY:
dee
,
powhatan, va
Overall rating:
5.0 out of 5
"I have the lighted keyboard and it does not stay on long enough to type in your password. As long as you keep typing, the light stays on, but the second your hands are off the keyboard the light goes off."
POSTED BY:
Kirsty
Overall rating:
1.0 out of 5
"Laptop purchased to replace a 4 year old Vaio and despite the supposed better processor, RAM, etc. we have been extremely disappointed with it's performance and avoid using it whenever possible. Biggest issue is the mouse pad which only responds around 30% of the time, followed by the battery which drains rapidly when the machine is switched off - usage on battery power is around 1 hour on a good day. The screen quality is also poor compared to the Vaio and also to a 6 year old Toshiba. Keypad also disappointing. Will be looking for a replacement very soon."
POSTED BY:
Reese
,
Sarasota, FL
Overall rating:
5.0 out of 5
"The Toshiba has a fast processorand a good amount of memory which results in a very satisfying performance."
POSTED BY:
CK
,
USA
Overall rating:
4.0 out of 5
"Great feature set at a good price point. The dimensions on the spec sheet are incorrect, the notebook is about an inch longer, so take this into consideration if you're ordering a case for it. I've had a few windows glitches with some memory dumps, but I think it's software related. Battery life is less than expected (about 2.5 - 3 hours run time). Spec sheet says you can get 6 hours, but that's if you dial everything back. LED backlit keyboard is nice, and the wireless has worked out great. The touchpad is picky on finger placement when scrolling. Overall, I'm pleased with this notebook. Also, you can purchase an extended warranty and accidental damage plan through Toshiba at a significant discount compared to what you can get from a big-box store."