Toshiba Satellite P770-ST5N01 Laptop

Satellite P770-ST5N01

MSRP: $979.99
Satellite P770-ST5N01 4.71 out of 5.0 based on 13 user reviews. Average Customer Rating: 4.71 out of 5.0
Read Reviews (13) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Satellite P770s that are available:
Satellite P770 Series »
Laptop Accessories
Shop for Satellite P770-ST5N01 accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite P770-ST5N01 or try our Laptop Forums for additional help.
Intel® Core™ i5 Processor
Accessories for the Satellite P770-ST5N01

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Satellite P770-ST5N01 Laptop Customer Reviews

Great!

POSTED BY: , Seto, Japan
Overall rating: 5.0 out of 5

"This is my second Toshiba Laptop, and they've always held up well, and can usually do everything I need them to."

Great laptop at great price

POSTED BY: , Boston, MA
Overall rating: 5.0 out of 5

"The Satellite P770 is a sturdy and well built laptop. The Core i5 processor allows you to run anything from basic WordDoc to games. The laptop is quiet and does not heat up. Toshiba has a international warranty which is another plus. Only disappointments are that the battery life is not very long compared to other brands and the already-built versions only have an integrated graphics card. Overall, its a great laptop with great value."

Nice desktop replacement

POSTED BY: , NYC
Overall rating: 5.0 out of 5

"My wife uses it mostly for internet surfing & online games (farmville type) and Skype. The camera & mic are good and the speakers seem really good for laptop speakers. The 17in screen is great. She says that with the cord unplugged the laptop only lasts about 1hr& half, but that's while playing a game."

Nice Laptop

POSTED BY: , Pittsburgh, Pa
Overall rating: 4.0 out of 5

"I'm not tech savvy but with this computer you don't need to be I was able to connect with my WiFi with no problems. I like the backlight keyboard. This is the first laptop that I have owned. It's very easy to work with, haven't used all of the features as of yet but if it's anything like what I've already discovered I foresee no problems."

Toshiba P770-ST5N01

POSTED BY: , TX
Overall rating: 5.0 out of 5

"I did a LOT of research before making the decision to buy this laptop. I LOVE it! The graphics are fantastic, processor speed is really good. I love the fact that the keys light up when you type making it easier to see. The screen is big! I am very happy with this laptop and would definitely recommend it to anyone!"

laptop

POSTED BY: , OakLawn,Il
Overall rating: 5.0 out of 5

"I love the back-lit keyboard."

Needs reboot often

POSTED BY: , Wilmington, NC
Overall rating: 4.0 out of 5

"Mouse and touchpad go wonky about 3 times per week rendering them unusable. The Microsoft mouse works fine on my other Toshiba laptop. Have deleted and reinstalled the mouse driver to no avail."

Very lite and long battery life.

POSTED BY: , Marysville,CA
Overall rating: 4.0 out of 5

"I was very surprised how lite this laptop was and the battery lasted alot longer than mt last Toshiba laptop. I like the lighted keyboard, it's what sold me on this laptop. The only thing I dislike is the touchpad. It is touchy, even after adjustment and my old laptop had a recessed lip around touchpad. Made it easier to find touchpad and know where you where. But overall I like it, it's fast and works great."

second laptop from Toshiba

POSTED BY: , Mena, Ar
Overall rating: 4.0 out of 5

"Weight is heavy for a laptop. There durible and dependable. Service is great. Window 7 will take sometime getting used to coming from XP. There great dependable computers. My old one is still going and it is a P100 Serice."

Best laptop ever

POSTED BY: , LAFAYETTE, LA
Overall rating: 5.0 out of 5

"The features are great. The back light is fantastic. The style looks even better than I thought"
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.