POSTED BY:
JW
,
Cascade Idho
Overall rating:
5.0 out of 5
"Like this laptop alot. Screen is very crisp and sharp. Plenty of storage and not to heavy."
POSTED BY:
Andy
,
Morton Grove, IL
Overall rating:
5.0 out of 5
"Its light weight but very fast. The battery seem to be better than what the reviews stated. The 17" screen is terrific."
POSTED BY:
Heber
,
Utah
Overall rating:
4.0 out of 5
"Really good computer, so far, the only reason that I gave a 4 star overall ( and an 3 in features) was because it came loaded with a bunch of extra software that I had to remove"
POSTED BY:
FATCATDETROIT
,
DETROIT, MI AREA
Overall rating:
4.0 out of 5
"SHOULD HAVE A LIGHTED KEYBOARD FOR THE PRICE. SHOULD HAVE LONGER BATTERY LIFE. SHOULD HAVE A CHOICE WHETHER TO GO TO TOSHIBA'S WEBSITE ON BOOT-UP, INSTEAD OF MANDATORY. KEYPAD TOO TOUCHY. HAVE LOST COMPLETE LETTERS WHEN TYPING BECAUSE OF THAT. GOOD PERFORMANCE."
POSTED BY:
ReligBookFreak
Overall rating:
3.0 out of 5
"Ever since I got this laptop, I have had issues with Windows 7 crashing (i.e., stopping and restarting). Also, the USB port on the right side of the laptop are in a bad location. I like to place my mouse (I use a standalone mouse) right next to the laptop (on the right side). However, that's exactly where two of the USB ports are located. Therefore, the USB cords plugged into those two ports prevent me from placing my mouse in the location I want it. More than 4 USB ports would be appreciated. Why only one USB 3.0 port? I don't need 3 USN 2.0 ports; I would rather have all the ports be 3.0. Not as fast as I would have expected for an i7-2670 processor."
POSTED BY:
Nathan
,
Half Moon Bay, CA
Overall rating:
5.0 out of 5
"This laptop has just about all the features anyone could ask for. Performance is awsome for home use and very good for office use. The sound system is better than average and it could use a better graphics card. All in all it is an awsome laptop for its price. Definitely more bang for the buck!"
POSTED BY:
Fatty
,
Maryland
Overall rating:
5.0 out of 5
"The satellite laptop I purchased had the options that I wanted. That being said I am not a gamer nor do I frequent social media websites. I have a great afinity for music and buy/download many albums a year. Sound quality is one feature that was important to me, this computer delivers. The high resolution screen and Blu Ray DVD were items that were considered as well. The laptop I replaced was a Sattellite of '04 vintage which never experienced a hardware malfunction. In fact the only time it was cracked open was to add RAM. In my opinon Toshiba has proven that quality is very important."
POSTED BY:
TOM
,
S SAN FARNCISCO
Overall rating:
5.0 out of 5
"HI THIS FIRST TIME I HAVE TOSHIBA WAS EXCELLENT... NO MORE HP NO MORE... TANK YOU TOSHIBA"
POSTED BY:
Slick50
,
Louisville KY
Overall rating:
2.0 out of 5
"The hardware is solid, but the casing leaves something to be desired. I purchased this machine to replace my home pc because I have always trusted Toshiba. . The unit arrived, I was very excited. Unboxed the machine and immediately did not like it. The battery in the back moves back and forth in one end. The escape key was pinched under the casing, when I grabbed the unit on one side I hard some popping sound some something was not quite in its place. I am sending this unit back and will wait, but then again I am SERIOUSLY thinking about buying a MAC instead. I should have listened to my instincts."