Toshiba Satellite P845T-S4310 Laptop

Satellite P845T-S4310

MSRP: $909.99
Satellite P845T-S4310 3.81 out of 5.0 based on 55 user reviews. Average Customer Rating: 3.81 out of 5.0
Read Reviews (55)  | Write Reviews
Intel® Core™ i5 Processor
Accessories for the Satellite P845T-S4310

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite P840 Series Laptops
P840
Model: MSRP:
P845T-S4305 $795.99
P845T-S4102 $886.99
P845T-S4310 $909.99
P840T-ST4N02 $1,079.99*

*ToshibaDirect Exclusive. Price includes applicable discounts.

Satellite P845T-S4310 Laptop Customer Reviews

Simple, classy, easy to use

POSTED BY: , Dracut, Mass
Overall rating: 4.0 out of 5

"I love the size, look, and overall performance of my Toshiba. I'm still working my way around it, learning more about it's features, but find the material made available by Toshiba is more than sufficient to do that."

Excellent Product

POSTED BY: , Albrightsville, PA
Overall rating: 5.0 out of 5

"I love this laptop. I struggled for 3 months with price, performance and value before I bought this laptop. Toshiba is the best. It out performs all the other laptops that I have had."

Great Laptop,Great Price

POSTED BY: , Yellowstone National Park
Overall rating: 4.0 out of 5

"I am very happy with my new Toshiba, it has a lot of useful features and runs very smooth and fast. I marked it lower on performance because of a little glitch I encountered soon after purchase. I had to reformat. I don't blame the manufacturer it was a windows 8 glitch. I would not give windows 8 a good review. Since that no more problems the laptop is great to use.The touch screen is the cherry on top ."

Nice laptop

POSTED BY: , Douglas, WY
Overall rating: 4.0 out of 5

"I like the weight of this laptop. I also like the touch screen. I am having trouble with the Windows 8 and all the changes there. Wish I had a book of directions. Also, the book that came with the laptop has the buttons all opposite of where they really are. I also wish it had more USB ports so I could plug in all my many apps etc. Overall it is a very nice laptop."

Great Experience

POSTED BY: , San Antonio, Tx
Overall rating: 4.0 out of 5

"has an attractive chasis and excellent audio. This touch lap is a good value."

Cool Laptop

POSTED BY: , Westminster,SC
Overall rating: 4.0 out of 5

"The laptop works well - I am very pleased with it - However very much dislike Windows 8 that came with the system. Love the light weight of this unit."

Unlucky maybe

POSTED BY: , Minneapolis, MN
Overall rating: 4.0 out of 5

"I first had a 17" Toshiba and loved it, but it was too big for my cases, so returned it for the 11.5". I liked the step by step set up directions, but in the AM, the laptop was dead. I returned it and was not confident to get another, so I'm still without a laptop."

Some issues

POSTED BY: , Washington DC
Overall rating: 4.0 out of 5

"Satisfied with everything but the new windows and the non-functioning clickpad buttons."

nice

POSTED BY: , ramsey
Overall rating: 3.0 out of 5

"taking a while to get used to touch screen. seems to be ok."

Everything you need in a Laptop!

POSTED BY: , Long Beach, CA
Overall rating: 4.0 out of 5

"Fast, sleek design, the best speakers.good value.."
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
  • P840
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.