Toshiba Satellite P850-BT3G22 Laptop

Satellite P850-BT3G22

  • List Price with Upgrades:
  • $1,129.99
  • Component Rebate:
  • -$170.00
  • Base List Price:
  • $959.99
  • Instant Savings:
  • -$100.00

Total Price:

$859.99

Start Customizing
Satellite P850-BT3G22 2.60 out of 5.0 based on 4 user reviews. Average Customer Rating: 2.60 out of 5.0
Read Reviews (4)  | Write Reviews
This product may be available at a local business reseller.

Find a Reseller

Accessories for the Satellite P850-BT3G22

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite P850 Series Laptops
P850
Model: MSRP:
P855-S5102 $725.99
P850-ST4NX1 $749.99*
P850-ST3N01 $899.99*
P850-ST4NX2 $899.99*
P850-ST4GX1 $1,049.99*
P850-BT3N22 $599.99**
P850-BT3G22 $859.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite P850-BT3G22 Laptop Customer Reviews

BE CAREFUL

POSTED BY: , Tinley Park IL
Overall rating: 1.0 out of 5

"Bougt this laptop in September, crashed % months later, I have to pay shipping costs back to Toshiba for repair, Im not a happy camper."

Physical Layout and Design

POSTED BY: , Sacramento, CA
Overall rating: 2.0 out of 5

"I bought this laptop because I could customize it with all the bells and whistles. I regret the purchase. Despite the high memory and speed, the design of the laptop itself is terrible. The trackpad is unpleasant to the touch and near impossible to use. A simple task such as dragging a file to the trash takes several tries. I have tweaked the mouse driver software to the best of it's ability, but the problem lies with the hardware. The keyboard casing is textured so even light brushing on the surface causes a vibration. It also hinders using the Windows 8 "off the screen" functions since the trackpad surface and casing surface are so different-- the items you drag simply "drop" before pulling off the screen. For the money, it would be much better to get a touch screen laptop than attempt to use this pre-Windows 8 'box' with the new operating system. The battery life is worse than my previous 6 year-old laptop. Additionally, the optical drive is flimsy and gets stuck to the point of not responding to software or hardware "eject" commands causing me to have to restart the laptop to retrieve CDs. The first few months of a new computer should be joyful, but the P850 feels like I'm using a hand-me-down from 2005."

best laptop ever

POSTED BY: , uae , dubai
Overall rating: 5.0 out of 5

"sooo nice laptop cant leavee ittt"

Bad hardware

POSTED BY: , MD
Overall rating: 1.0 out of 5

"Within a half hour of using it the screen got a purple tint to it. This tint was present in the Bios menu as well, so definitely not an operating system issue, but rather a hardware issues. I found the touchpad to be horrible to use as well. I returned it and got a full refund. The return process was relatively easy and they pre-paid the shipping. So, that part was good."
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
  • P850
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.