Toshiba Satellite S855-S5378 Laptop

Satellite S855-S5378

MSRP: $769.99
Satellite S855-S5378 4.03 out of 5.0 based on 145 user reviews. Average Customer Rating: 4.03 out of 5.0
Read Reviews (145)  | Write Reviews
Intel® Core i7 Processor
Customize your S850 at ToshibaDirect.com

Customize

Accessories for the Satellite S855-S5378

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite S850 Series Laptops
S850
Model: MSRP:
S855D-S5120 $588.99
S855D-S5148 $639.99
S855-S5369 $669.99
S855-S5377N $699.99
S855-S5164 $749.99
S855-S5378 $769.99
S855-S5168 $799.99
S855-S5380 $799.99
S855-S5188 $869.99
S855-S5381 $869.99
S855-S5386 $869.99
S855-S5170 $879.99
S855-S5165 $899.99
S855-S5384 $899.99
S855-S5382 $949.99
S850-BT3N22 $549.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite S855-S5378 Laptop Customer Reviews

Very nice computer

POSTED BY: , Cheyenne, WY
Overall rating: 4.0 out of 5

"This computer would be the best I've ever had except for Windows 8 which is weird. I had a computer consultant add a "Start" button so I can at least use the thing. The developers of Windows 8 are focused on photos & videos instead of doing business."

Frustrated

POSTED BY: , Milton, WA
Overall rating: 2.0 out of 5

"The first one I brought home had someone else's name set up on the hard drive. I returned it. The second one (the one I have now) has one big issue. The mouse pad freezes up the curser after I get to the start page. I had to connect a wireless mouse to the computer to get it to work. Considering returning it. I have only had it a few weeks."

Great Processing Speed

POSTED BY: , Dallas, Tx
Overall rating: 5.0 out of 5

"I purchased this model for the i7 processor. I am glad to say that I am very pleased with the processing speed of the laptop. It handles the video editing software program Lightworks by Editshare without lagging when processing the h.264 files, my previous computer could not handle this. OK, a couple of dislikes 1. The keys are a bit too fragile. 2. The memory card slot only accepts SD cards, would rather have it capable of accepting micro sd, xd, etc type of cards as well. 3. The battery life on my laptop is not as long as I hoped for, have to recharge it far too often. 4. There is too much Toshiba generated software pre-loaded on the computer. 5. Seems like the internal fan works overtime sometimes, might need better ventilation. Now for some Likes: 1. Processing Speed! 2. Descent Price for what you get. 3. Has a number keypad, which I use a lot! 4. Weight is OK. 5. Screen looks great. 6. Adequate sized storage on hard drive. 7, DVD/CD ROM plays great, with good speed."

Great Value

POSTED BY: , Tempe, Arizona
Overall rating: 5.0 out of 5

"Enjoy the Toshiba laptop. Lot of good features at a great value. Screen has good clarity, easy to use."

Best Price/Performance Laptop

POSTED BY: , Arica,CL
Overall rating: 5.0 out of 5

"Excellent Laptop, I have it from a month ago, all my programs run like a charm, autocad, matlab, etc. The bad thing is the keyboard, you have to press the keys hard, but is ok."

Great laptop

POSTED BY: , Sterling Heights, MI
Overall rating: 5.0 out of 5

"I am very happy with my new laptop and am even surprisingly used to the Windows 8 already. The laptop has a beautiful look and feel and runs very well. I got it for myself but my 6 year old daughter has also taken a liking to it. She loves the Windows 8 start menu ease of access for all of her websites. The battery life is particularly good as advertised."

So far, so good!

POSTED BY: , Pearland, Texas
Overall rating: 5.0 out of 5

"It was an adjustment for me to go from a desktop to a laptop for all my projects. I've only had this for a few weeks but I like the large screen, and the keyboard feels "natural". I've never really liked the mouse pad on other laptops, but I like this one. I feel like I have more control. Windows 8 is an adjustment too, but so far I'm loving my new Toshiba!"

Perfect Solution

POSTED BY: , Fort Lauderale, FL
Overall rating: 5.0 out of 5

"Best laptop solution for work applications"

Has issues, but ok.

POSTED BY:
Overall rating: 4.0 out of 5

"The computer is fine. Wish it came with a paper user guide, because when the computer goes down, I can't use the virtual user guide, can I? I HAAAAATE the no start menu. Sometimes I just leave it on , as I can't get it to show me icons with which I may get it turned off!!!!!!!!!!!!!! I HAATE Windows 8. Is Windows listening? It seems Windows gets worse every time they come up with a new one. Clearly, they are not listening to users."

Just Ok

POSTED BY: , Puyallup
Overall rating: 4.0 out of 5

"Good home user laptop at a decent price"
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
  • S850
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.