Toshiba Satellite S855-S5381 Laptop

Satellite S855-S5381

MSRP: $869.99
Satellite S855-S5381 3.91 out of 5.0 based on 22 user reviews. Average Customer Rating: 3.91 out of 5.0
Read Reviews (22)  | Write Reviews
Intel® Core i7 Processor
Customize your S850 at ToshibaDirect.com

Customize

Accessories for the Satellite S855-S5381

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite S850 Series Laptops
S850
Model: MSRP:
S855D-S5120 $588.99
S855D-S5148 $639.99
S855-S5369 $669.99
S855-S5377N $699.99
S855-S5164 $749.99
S855-S5378 $769.99
S855-S5168 $799.99
S855-S5380 $799.99
S855-S5188 $869.99
S855-S5381 $869.99
S855-S5386 $869.99
S855-S5170 $879.99
S855-S5165 $899.99
S855-S5384 $899.99
S855-S5382 $949.99
S850-BT3N22 $549.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite S855-S5381 Laptop Customer Reviews

Great after replacing original laptop.

POSTED BY: , Fredericksburg, VA
Overall rating: 4.0 out of 5

"The original laptop keyboard randomly lost typed characters. After about 10 days, I tried the store sample and was convinced that the problem was with my laptop. The store had no unused replacements, so I returned my laptop to the store and bought another identical unit at another store. Wasted a good week of my time, but I am fully satisfied with my new laptop."

Good Laptop except for the keypad

POSTED BY:
Overall rating: 3.0 out of 5

"The keyboard is not very user friendly, lot of missed keystrokes."

Excellent Laptop

POSTED BY: , Matlacha, FL
Overall rating: 5.0 out of 5

"It was time for me to upgrade to a laptop with better performance. I researched a number of vendors and decided on Toshiba for a couple of reasons. The main reason being the i7 chip, quad core, exceptional storage and very easy to use keyboard."

at one is was toshiba but???????

POSTED BY: , North Kingstown RI
Overall rating: 4.0 out of 5

"It would been nice if we had a book about your computer next timei I will check to see if a book telling as about your computer."

woudn,t buy it again

POSTED BY: , ct
Overall rating: 3.0 out of 5

"to many things preloaded making navagation hard"

Spoiled only by Windows 8 being installed

POSTED BY: , Buffalo, NY
Overall rating: 3.0 out of 5

"This is my third Toshiba laptop. They are excellent machines! I wish I could have found one with Windows 7 installed but there were none to be found. So I purchased one with the truly awful Windows 8, thinking that it might not be as bad as I had heard. In fact it wasn't as bad as I'd heard, it was much much worse. The many and various popups and things that slide across the screen all the time simply serve to spoil my workflow. So I had to buy a copy of Windows 7 Pro, uninstall Win 8, and upgrade my Toshiba to Windows 7. Now I have a fabulous machine! It works like a dream!"

Think again

POSTED BY: , Plano, TX
Overall rating: 3.0 out of 5

"Working in a one to one computer school I have been given many Toshiba computers for 7+years. I did not think twice about purchasing one for myself and all the school work I do at home. I like the 15.6" screen and battery life of my S855. However, with the higher price, I thought I was getting better quality. The keyboard is such poor quality. It is flimsy, sticks, and often locks up on me."

Very good price for value!

POSTED BY: , Europe
Overall rating: 4.0 out of 5

"Very well designed, easy to use, very good price for value ratio. Excellent performance. The Toshiba software that comes with the Laptop could have been better. The DVD-RW is a bit loose. I'd recommend this product to every one."

Fantastic system

POSTED BY: , Boca Raton, FL
Overall rating: 5.0 out of 5

"Just an awesome system. With the Core i7, 8GB DDR3 1600MHz memory and 1TB of disc, and the price; just incredible. Fast and very good looking machine. My third Toshiba and it continues to impress."

Good performer

POSTED BY: , Albuquerque, NM
Overall rating: 4.0 out of 5

"I have had this computer for a while and there is honestly only one thing I don't like about it.The touchpad isn't as responsive as it should be for multiple finger gestures. Other than that it has been great."
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
  • S850
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.