Toshiba Satellite S875-S7356 Laptop

Satellite S875-S7356

MSRP: $749.99
Satellite S875-S7356 4.50 out of 5.0 based on 6 user reviews. Average Customer Rating: 4.50 out of 5.0
Read Reviews (6)  | Write Reviews
Intel® Core™ i5 Processor
Customize your S870 at ToshibaDirect.com

Customize

Accessories for the Satellite S875-S7356

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite S870 Series Laptops
S870
Model: MSRP:
S875-S7356 $749.99
S875D-S7350 $749.99
S875-S7376 $999.99
S870-BT3N22 $599.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite S875-S7356 Laptop Customer Reviews

first laptop and it is great !!!!!

POSTED BY: , chicopee ma.
Overall rating: 5.0 out of 5

"Easy to use. but windows 8 is hard to get used to."

I like it now i understant it

POSTED BY: , Has Hgts N.J.
Overall rating: 3.0 out of 5

"iTS WAY DIFFERENT FROM WIN 7. And I am still getting use to it, I just wish it worked with my Plam T 5"

Excellent Laptop

POSTED BY: , Burleson, TX
Overall rating: 5.0 out of 5

"This laptop performs above my expectations. Loads up fast, runs programs good. Very good product overall."

Godd value

POSTED BY: , new jersey
Overall rating: 4.0 out of 5

"Very good laptop for the money some nice features"

Great Laptop at a Great Price

POSTED BY: , Brooklyn, NY
Overall rating: 5.0 out of 5

"Very good product. Loaded with features, 17.3 inch screen is wonderful, although it could be sharper; although I am comparing the screen quality to my Samsung Smart TV, which is 1080p @ 120/hz. Large touch pad makes using it comfortable. The screen could be higher, one of my few complaints. It also didn't come with a Blu-Ray disc drive. It would be nice to offer a Blu-Ray writer option as well. Overall, this is a great product I will recommend to my family and friends. Great, reliable performance and a user friendly interface offered by the pre-loaded Windows 8 operating system."

Nice Laptop

POSTED BY: , McAllen, Tx
Overall rating: 5.0 out of 5

"Over all it is a solid laptop with a nice solid look. I am still trying to get used to windows 8 but over all it is very responsive, have not had trouble with lag or being to slow. I mainly use it for Dj and its screen is big enough to do the job. I actually didn't realize how big the screen really was. If you are looking for something more portable then this is not really meant for you. The battery life is not log either but it will last you a couple of hours. Over all I would recommend to anyone."
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
  • S870
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.