Toshiba Satellite S875D-S7350 Laptop

Satellite S875D-S7350

MSRP: $749.99
Satellite S875D-S7350 4.20 out of 5.0 based on 10 user reviews. Average Customer Rating: 4.20 out of 5.0
Read Reviews (10)  | Write Reviews
AMD Vision A10
Customize your S870 at ToshibaDirect.com

Customize

Accessories for the Satellite S875D-S7350

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite S870 Series Laptops
S870
Model: MSRP:
S875-S7356 $749.99
S875D-S7350 $749.99
S875-S7376 $999.99
S870-BT3N22 $599.99**

*ToshibaDirect Exclusive. Price includes applicable discounts.

**Customizable laptop. Price shown is for base configuration and includes any applicable discounts. Price may change based on customization.

Satellite S875D-S7350 Laptop Customer Reviews

Not as good as my last Toshiba

POSTED BY: , Kentucky
Overall rating: 3.0 out of 5

"I have constant issues logging in to the internet, I am always having to reboot the laptop for whatever reason. My last Toshiba laptop was amazing for 6 years. Very disappointed with this one."

Great Laptop with a few issues

POSTED BY: , Palm Harbor, Fl
Overall rating: 4.0 out of 5

"So I got this laptop to do some office work on as well as some light gaming and ended up using it as my main computer. The laptop is fairly light and seems to run fairly cool unlike some other laptops which I have used that have burned my leg just sitting on my lap for an extended time. On the work side everything works as you would expect but on the gaming side I have been really impressed. It has run games I wouldn't think it would have like a champ, and even though I might not be able to run some on Ultra settings being able to game on the go with settings on medium and 30-42 fps is pretty nice. The only issues I have run into so far is the track pad and the wireless card. Every now the track pad will go unresponsive for no apparent reason. This isn't too big a deal for me as I use a wireless mouse and don't run into the problem with it, but it is still an issue and I might just need to update drivers but I'm pretty sure they are all current. The other issue is the wireless card. It seems to not see my network every now and then. Seems like I have to uninstall the device form the manage hardware and reboot and it will pick it back up. Now this might be my router through FiOS or it might be the card. At any rate both of those issues have been the reason for the 4 star rating and not a 5. If you are looking for a great laptop this Toshiba seems to be a good solid laptop. I haven't had a game it hasn't been able to handle yet and I have been more the happy with the performance and battery life. Now Windows 8...that is another story but I am getting used to it."

very good laptop

POSTED BY: , 28504
Overall rating: 4.0 out of 5

"I like the 17" monitor for viewing multiple apps"

love it

POSTED BY: , clearlake oaks , ca
Overall rating: 5.0 out of 5

"I found this unit online , and bought it , very happy"

mediocre

POSTED BY: , Colorado
Overall rating: 2.0 out of 5

"USB3 seems buggy, never get it to work with the EZ-Dock2 HDD dock. Prrocessor virtualization disabled? makes VMWare painfully slow. Windows 8 ... not a big fan. Don't like the gouped function keys, makes it difficult for those of use who use F5 and F3 a lot. Has good speed and battery life."

POSTED BY: , Bensalem, Pa.
Overall rating: 5.0 out of 5

"Meets all expectations. Does everything as stated and more"

Great Laptop

POSTED BY:
Overall rating: 5.0 out of 5

"I have only had this laptop for a few weeks, but thus far loving it. It is very fast."

Nice power-packed laptop!

POSTED BY: , Chickamauga, GA
Overall rating: 5.0 out of 5

"The S875D-S7350 is a nice laptop. I love the large 17.3 inch screen but it seems to not kill the battery even with such a large screen. It loads up fast thanks to the RAM and I can run multiple programs due to the quad-core processor. One of the best features is the HDMI output which allows me to hook the computer up to my HDTV to use as a second monitor. I also really like that it has a Blu-Ray player. Overall, this is a great laptop that packs a lot of features for a great price!"

I'm an Old Dog who has Trouble with New Tricks

POSTED BY: , Round Rock, TX
Overall rating: 4.0 out of 5

"I wanted a Laptop with lots of memory for my online game as well as good with photos. The graphics are wonderful for my game. I absolutely, positively HATE Windows 8. I have used the same Road Runner Email for over 10 years and Windows 8 does not support that type of email server and I was forced to use Outlook in order to maintain my existing email address. There was no editing software for my photos with the laptop and Windows 8 does not display the photo properties (comments, etc) like Windows XP or Windows 7 so I was a little horrified with that. I travel the world and like to put a comment on each photo so in 10 years I'll know what it is. The keyboard is great, love the 10 key pad. Not a big fan of the dual function F keys. I still use the F keys and it is a pain to have to Shift to get to them."

Great laptop!

POSTED BY:
Overall rating: 5.0 out of 5

"Awesome laptop for gamers, but if you like to max out all of your settings then you probably don't want this. Games such as Borderlands 2 will ran on medium settings and things like bloom, flares, etc.at 30 FPS. That's pretty awesome for a laptop of this price. The application updater tool included is a neat feature where I can see and update things like my graphic card and other drivers. Only problem I've had so far is that the realtek wireless LAN driver downloaded from the application updater is really buggy and you'll probably have to do a system restore if you install it."
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
  • S870
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.