MSRP†: $479.99
Average Customer Rating:

Read Reviews (7)

Carrying Cases
Batteries
AC Adapters
Memory
Docking & Expansion
| Model: | MSRP: |
|---|---|
| T115D-S1120RD $449.99 | |
| T115D-S1125RD $499.99 | |
| T135D-S1326 $599.99 | |
| T135D-S1325WH $599.99 | |
| T135-S1310 $699.99 | |
POSTED BY:
jdinps
,
Palm Springs
Overall rating:
4.0 out of 5
"This pc handles multiple programs a netbook would not be capable of handling. The core processor is a Pentium for this little guy and I wish it were a dual core for faster processing, but it handles my needs adequately. I would recommend this laptop to anyone who needs a small lightweight laptop with the ability and memory to handle multiple software apps for business."
POSTED BY:
keltora
,
Knoxville, TN
Overall rating:
5.0 out of 5
"As an author, I am always looking for a machine that is light and portable and reasonably priced, but able to leap tall building (just kidding) and be the perfect travel companion. I have found it in this particular model. I don't care if it doesn't have an optical drive. I use it for writing on the road and checking email, and occasionally playing games while I am "thinking" up my next novel. So thank you, Toshiba, for finally answering my prayers. I guess I will be looking for homes for a couple of netbooks now..."
POSTED BY:
Bill
,
Madison, WI
Overall rating:
4.0 out of 5
"I bought the Toshiba Satellite T115-S1105 because it is as portable as a netbook, but (almost) as fast and powerful as a laptop, with screen size in between and battery life much better than either catagory. Thanks to HDMI output it is now connected to a good monitor with good speakers and has also replaced my desktop. This laptop is very portable with excellent battery life. Excellent screen resolution, reasonable hard disk capacity and storage. Fast DDR3 memory in adequate amounts. The Pentium SU2700 could be faster, but is acceptable for net surfing, email, letter and report writing, average sized spreadsheets and powerpoints. I repartioned the hard disk and placed the Linux distro Ubuntu 9.04 as primary boot; now it runs faster and I prefer Ubuntu to Microsoft."
POSTED BY:
susan
,
nj
Overall rating:
3.0 out of 5
"i am considering taking it back to the store its slow sometimes. the volume in this computor is terrible i cant even hear it at all. i hope they do not give me a hard time when i return it. i also have a hard time with the internet takes a long time to get on always tells me there is a connection problem."
POSTED BY:
SOLOLAPTOP
,
indonesia
Overall rating:
4.0 out of 5
"this model very excelent. it has ddr3, windows 7, and intel chipset. ddr3? wow. first time in netbook."
POSTED BY:
SPA2TACU5
,
USA & Netherlands
Overall rating:
2.0 out of 5
"So far the touchpad is horrible. It hardly reacts, or will only move vertical, or horizontal, or will resize the browser font size, or won't move at all, or will drag 'n drop things... The sound seems to be very low. Everything set to full through Windows 7 sound control. I'm trying to figure out if there's another sound control somewhere that's still set to low. The "FN"key + the vol up and down keys (3 and 4) are not working. Personally I don't like the high glare case. Attracts a lot of dust. Plus: good spacey keyboard, nice screen, pretty fast boot-up and shut-down. NB I´ve been using an Asus EEE pc 701 (Linux) since jan ´08."
POSTED BY:
bk
,
Paramus Nj
Overall rating:
1.0 out of 5
"Loaded all. backed up and rebooted. Blank screen with mouse pointer only visible. Read about windows 7 problems, and using f8 started with low resolution. Then it stuck with starting Toshiba regstration."