Toshiba Satellite T135-S1310RD Laptop

Satellite T135-S1310RD

MSRP: $699.99 Satellite T135-S1310RD 4.20 out of 5.0 based on 10 user reviews. Average Customer Rating: 4.20 out of 5.0
Read Reviews (10) 

This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
mini notebook NB500 Series »
Laptop Accessories
Shop for Satellite T135-S1310RD accessories at ToshibaDirect.com.
Technical Support
Get support for your Satellite T135-S1310RD or try our Laptop Forums for additional help.
Intel® Pentium® Processor
Accessories for the Satellite T135-S1310RD

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Available Satellite T100 Series Laptops
T100
Model: MSRP:
T115D-S1120RD $449.99
T115D-S1125RD $499.99
T135D-S1326 $599.99
T135D-S1325WH $599.99
T135-S1310 $699.99

Satellite T135-S1310RD Laptop Customer Reviews

Good Machine so far

POSTED BY: , RI
Overall rating: 4.0 out of 5

"I bought this used for my wife. It seemed to be at least $100 below market value for a used machine. I exclusively bought Dells in the 90's and HP in the 2000's but based on this unit I would defin. consider a Toshiba in the future."

10/10 Awesome!!! Great!!!

POSTED BY:
Overall rating: 5.0 out of 5

"First, I want to say that this laptop does not have any problem with the speakers as many computer web pages say. Only it was a problem with windows 7! so after updating the laptop with the package offered by Toshiba, now no problem with the speakers!! Awesome, great, 10 to this laptop!!!"

POSTED BY: , Los Angeles
Overall rating: 1.0 out of 5

"This is my second Toshiba laptop. I have never had a problem with the first one and only purchased this new one (after 6 years) only because it would have cost too much to fix the other one. Having said that, the machine itself is great - the color, it's light weight, the battery lasts a long time, etc. Unfortunately, it comes installed with Windows 7 and I have had nothing but technical difficulties with the operating system and the programs preinstalled with the computer. For instance, the first week I had it, the taskbar would disappear. Then after I was able to finally fix that problem, another problem arose with microsoft word, excel, and power point presentation programs. I kept having problems (still having problems) opening up programs directly in word, excel, or power point. I keep getting an error message. Then I had problems installing a program into my laptop that is compatible with word. Even now, I am unable to install a HP printer because for some reason it is stating that the version 5 or higher of internet explorer needs to be installed. Well, guess what? This is a new machine. I should have the newest version of internet explorer. Honestly, I wish I had returned or exchanged the machine when I still had the chance and it was within the 30 days. Don't buy, not worth all the trouble."

Perfect Travel Companion

POSTED BY: , ST. LOUIS
Overall rating: 5.0 out of 5

"I researched my purchase for several weeks and finally bought this model in early March. This model has it all--lightweight, resolution, 64 bit windows, bluetooth, speed and a great battery. I debated buying the NB305-410BL netbook. I'm glad I bought this slightly larger computer because it's has all the qualities of a netbook with better performance, resolution and potential. I have not had any technical issues. I went to the Toshiba website and ensured it had all the latest drivers and software. I did have to update the sound driver for the sound level but it was no problem. I recently purchased a Mobile Edge case .Mobile Edge MESSM7-13 13-Inch Neoprene SlipSuit (Red) to protect it. The case is made for the Macbook but fits great around this T135-S1310 plus it has a pocket for some smaller devices. The AC cord will not fit but I store it in another area when I travel. I definitely would purchase this product again"

Great little machine.

POSTED BY: , Azusa, CA
Overall rating: 4.0 out of 5

"I really enjoy my gorgeous red laptop a lot. The size 13.3" and reduced weight makes it useful to take on trips. Toshiba's update on the volume helps a lot. The screen is nice and bright. The typing keys are a good size but typing is a bit spongy (the keyboard moves) The sound for music is tinny, but that seems to be a problem with most laptops. I do like the installed Windows7. This little laptop is faster than my HP big laptop. I purchased the Toshiba external DVD player since there is no DVD/CD player installed. The external player is rather noisy but it works to install software etc. All in all I am very pleased with my purchase."

Great Laptop

POSTED BY: , New Hope, PA
Overall rating: 5.0 out of 5

"My only disappointment is the life of the battery. I should have asked to have the 12 cell instead of the ? one included as shipped. Love the keyboard and keys, better than my HP.I find it comfortable. Screen is great too! The battery life is not what I expected"

Excellent Performance Overall

POSTED BY: , Pittsburgh, PA
Overall rating: 5.0 out of 5

"The Satellite T135 is a powerful laptop in a lightweight and stylish package. I have been very pleased with it's features and performance overall."

Sleek!

POSTED BY: , Colorado
Overall rating: 4.0 out of 5

"This laptop is sleek, lightweight, fast & versatile. My only complaint is the sound....just doesn't get loud enough. Sometimes I have to pick it up and hold it close to hear what's it's saying."

Best Travel Laptop

POSTED BY: , Torrance, CA
Overall rating: 4.0 out of 5

"It's best for internet and travel laptop. The performance is average because of the energy saving on the laptop. I need this style, but with the faster performance. It's slow, when opening. It work well, once it's operated."

Very BEST!

POSTED BY: , Moscow, Russia
Overall rating: 5.0 out of 5

"T135 have all that i need to the road."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Satellite Laptops
  • L735 for kidsL735 for kids
    Satellite® L735 for kids
    Built-in parental controls
    Built for tough handling
    Compact child-friendly size
    Pre-loaded kid-centered entertainment
    Toshiba quality and reliability
    Starts at: $505.99
  • L730L730
    Satellite® L730
    Lightweight and easy to carry
    Amply sized, mobility-minded display
    Renowned Toshiba styling
    Eco-consciously engineered
    Packed with Toshiba Smart Features
    Starts at: $529.99
  • E305E305
    Satellite® E305
    Lightweight laptop
    Designed with your expectations in mind
    Delivers performance-driven mobility
    Allows more wireless freedom
    Premium style and design
    Starts at: $949.99
  • L740L740
    Satellite® L740
    Simplifies everyday computing
    Sized for on-the-go multitasking
    Great for enjoying and sharing multimedia
    Offers famous Toshiba styling
    Packed with Toshiba Smart Features
    Starts at: $479.99
  • P740P740
    Satellite® P740
    Strong entertainment-focused performance
    Compact, portable design
    Latest-and-greatest technology
    Sleek, elegant styling
    Packed with Toshiba extras
    Starts at: $649.99
  • R845R845
    Satellite® R845
    Geared for all-out mobile performance
    Designed for on-the-go pros
    Highly durable and reliable
    Thin, light and stylish
    Extended battery life rating
    Starts at: $799.99
  • C650C650
    Satellite® C650
    Packed with laptop essentials
    Extremely affordable
    Larger display for movies or multitasking
    Famous Toshiba style and quality
    Geared for sharing media
    Starts at: $353.99
  • L750L750
    Satellite® L750
    Perfect for everyday computing
    Generous screen for movies or multitasking
    Famous Toshiba style and quality
    Made for easy sharing and expansion
    Packed with Toshiba Smart Features
    Starts at: $499.99
  • P750P750
    Satellite® P750
    Brilliant optional 3D viewing
    Performance tailored for entertainment
    Superb styling
    New-to-market technology
    Loaded with Toshiba extras
    Starts at: $679.99
  • C670C670
    Satellite® C670
    Packed with laptop essentials
    Very budget-friendly
    Extra-large display
    Celebrated Toshiba style and quality
    Great for connectivity and sharing
    Starts at: $447.99
  • L770L770
    Satellite® L770
    Expansive display for movies or multitasking
    Ideal for replacing a desktop computer
    Tailored for high-def entertainment
    Famous Toshiba style and quality
    Toshiba Smart Features for exceptional convenience
    Starts at: $532.99
  • P770P770
    Satellite® P770
    Broad, brilliant viewing
    Entertainment-focused performance
    Exceptional styling
    Latest-and-greatest technology
    Lots of Toshiba extras
    Starts at: $729.99

Toshiba Product Locator

xhide feature

Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Computers »

Laptops
Satellite®
Tecra®
Qosmio®
Portégé®
Customizable Laptops
Desktops
All-in-One Desktops
Hard Drives and Storage
Desktop External Drives
Portable External Drives
Accessories
dynadock®
Mobile Monitor
See All Accessories
Need Help Choosing A PC?
Laptop Finder
Computer Research Center

Tablets »

Excite™ Tablet
Thrive™ Tablet
Tablet Accessories
Tablet Finder

Televisions »

Internet Televisions
3D Televisions
LED Televisions
LCD Televisions
TV/DVD Combos
TV Accessories
Need Help Choosing A TV?
TV Finder
TV Research Center

Video & Electronics »

Blu-ray Players
DVD Players
DVD Recorders
Camcorders
Electronics Accessories

Explore Toshiba »

Our History
Contact Us
Social Responsibility
Careers
Ways to Buy
Toshiba Events
Our Commercials
Press Room
Reseller Partners
Public/Private Sector
Connect
Connect with us
Connect with us on Facebook Connect with us on Twitter Connect with us on YouTube