x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Satellite® U840t Series

starting at: $ Shop U840 Series

14” Satellite<sup>®</sup> U840t Ultrabook Series

Satellite® U840

5 models available Starting at $799.99 $799.99
$899.99
Satellite® U840 4.57 out of 5.0 based on 7 user reviews.

Customer Reviews for Satellite® U840

Not my dream machine but close

POSTED BY: , Tuscaloosa, al
For Model: Satellite U845T-S4165
Overall rating: 5.0 out of 5

"This laptop has great specs just wish the hard drive was bigger and the memory bay was easier to access."

U845T-S4165 is a GREAT little laptop!

POSTED BY: , Albuquerque, NM
For Model: Satellite U845T-S4165
Overall rating: 5.0 out of 5

"The U845T-S4165 is a simple little laptop. In the 14 inch class, it was the right size for my mobile use. I installed it in a pickup and use it for radio communications control. The touchscreen with Windows 8 is very efficient when a mouse can't be used during mobile operations. Furthermore, the solid state drive (SSD) is ideal for the rough roads I sometimes have to travel. That would be tough on a hard disk drive. It performs well with Windows 8 and overall I'm very satisfied with this little laptop. This is my 5th Toshiba laptop and I've always been happy with them. However, this was my first purchase via Toshiba Direct and I'm happy with their service too. There were no comparable PCs to found locally or at other sites. The price seemed fair, but I hope the cost of touchscreens and SSDs comes down. I will definitely consider Toshiba Direct again for my next purchase."

Nice Laptop

POSTED BY:
For Model: Satellite U845T-S4155
Overall rating: 4.0 out of 5

"Purchase because I wanted little larger screen than a standard 13.3 and did not want the weigh of a 15.6 laptop. Lighted keyboard is nice. Rubber stopper and screws are falling out of the bottom though. I payed below retail so I'm very happy with the value. SSD drive makes for a quick start up."

Excellent laptop. Value for money

POSTED BY: , Australia
For Model: Satellite U845T-S4165
Overall rating: 5.0 out of 5

"I am very pleased with this product. Although I did not have much time to use it , during the short time I used it , it rally impressed me with all it's features. I had an expensive competitive product (tablet)which I had to return due it its poor performance. BUT U845T-S4165, delivered what it promised at a fraction of the price. Great product! Highly recommended. Real value for money."

Wonderful Ultrabook

POSTED BY: , Ohio
For Model: Satellite U845T-S4165
Overall rating: 5.0 out of 5

"I have used for one month and love everything about my Satellite U845T. Just the right size, feel and backlite keyboard works great when working in dark area of my house"

A good cafe cruiser.

POSTED BY: , AZ
For Model: Satellite U845-S404
Overall rating: 3.0 out of 5

"This model of Toshiba ultra book is great for browsing the web or writing documents. Although it comes with the Intel HD 4000 chip set, it is not for gaming. It is small and light, and the battery performance is acceptable. Compared to today's ultra books though, this is not worth the price. To get the most out of this computer, I recommend upgrading to windows 8. Battery life and performance will increase greatly!"

super ultrabook

POSTED BY:
For Model: Satellite U845-S404
Overall rating: 5.0 out of 5

"i try many brands in ultrabook but this is the best"

Customize or choose a pre-configured Satellite® U840 »

starting at:
$
Shop U840 Series
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
  • U840