Toshiba Satellite U925T-S2300 Laptop

Satellite U925T-S2300
Ultrabook™ Convertible

  • List Price:
  • $1,149.99
  • Instant Savings:
  • -$150.00

Total Price:

$999.99

Buy Now
Satellite U925T-S2300 4.12 out of 5.0 based on 7 user reviews. Average Customer Rating: 4.12 out of 5.0
Read Reviews (7)  | Write Reviews
Intel® Core™ i5 Processor
Accessories for the Satellite U925T-S2300

Accessories
Carrying Cases
AC Adapters
Docking & Expansion

More Satellite U920T Series Laptops
U920T
Model: MSRP:
U925T-S2120 $870.99
U925T-S2100 $998.99
U925T-S2130 $999.99
U925T-S2300 $999.99
U925T-S2301 $1,149.99

Satellite U925T-S2300 Laptop Customer Reviews

Good idea but heavy

POSTED BY: , Fort Worth TX
Overall rating: 4.0 out of 5

"The idea of multile positions is good, but is worrisome. The screen is sometimes difficult to handle. I am concerened about the life of the tracks and the hindges."

Overall great product!

POSTED BY: , Alexandria, VA
Overall rating: 4.0 out of 5

"I love the fact that this product converts from a laptop to a tablet. It's lightweight, easy to use, and the light-up keyboard feature is nice to have. One thing that I would have liked to see is the availability to use the rear-facing camera when the device is collapsed as a tablet. The rear camera is only exposed in laptop mode, making it difficult to snap pictures and hold the device at the same time."

Valid Experiment. Falls Short.

POSTED BY: , New York, NY
Overall rating: 3.0 out of 5

"As a longtime slider phone user (need that qwerty keybard!) thought I'd try the U925t as my first Win 8 experience. Feelings mixed so far. As a laptop it's fine, but dark screen & low def make it not great for media. Price also too high for what it is."

Awesome laptop/tablet!

POSTED BY: , Haines, AK
Overall rating: 5.0 out of 5

"This laptop is so easy to use. I am not very computer tech but have no problems getting where I wish to go. Love the touch screen! And being able to fold it up into a tablet is awesome!"

Excellent buy

POSTED BY: , Marion, IL
Overall rating: 5.0 out of 5

"This has got to be one of the best purchases I ever made! The computer is very light and the new Windows 8 operating system runs fast compared to older versions. Well, I have to admit Windows 7 is great also but this offers much more with the tiles. You have to get this touch screen because trust me, I loaded the trial version of 8 on my other laptop and it’s just not the same using a keyboard and mouse. Granted, it is lacking some apps but more and more are getting added daily. I have tried iPad and this is operating system is going to create havoc for the Apples system. They made many improvements with security with Defender and other parts of the system. I love the way it slides back and forth where you can use it as regular laptop or tablet. The battery life is good and 5 to 6 hours life is good enough for me. It is solid and has a great feel to it where you can take it with you with no worries of dropping it. The 128 GB SS drive plus the Sky drive will hold all my work files and more. Also with Sky drive, you keep all those offline where they are safe in case something happens. If you are in to music it will work for you also. I am not in to gaming that much but it does most of my games good like words with friends and angry birds. The keyboard is great and lights up only when you using it to conserve battery power. One negative I can find is that the battery is internal and just can’t be replaced unless you take apart the computer. Once you start learning Windows 8 you will get the hang of it quickly because I am learning different things every day. One thing I just recently learned was in the apps you can find all those other items programs that are offered in Windows 7 like word pad and media player and maintenance functions. The screen size works for me because I watch movies on it when I am on the road from HBO, Netflix and Hulu and definitely like to see it on a bigger screen than say a 7 inch. The Toshiba is a great buy and sure you won’t be disappointed."

Very nice

POSTED BY: , Marion, IL
Overall rating: 4.0 out of 5

"This has got to be one of the best purchases I ever made! The computer is very light and the new Windows 8 operating system runs fast compared to older versions. Well, I have to admit Windows 7 is great also but this offers much more with the tiles. You have to get this touch screen because trust me, I loaded the trial version of 8 on my other laptop and it’s just not the same using a keyboard and mouse. Granted, it is lacking some apps but more and more are getting added daily. I have tried iPad and this is operating system is going to create havoc for the Apples system. They made many improvements with security with Defender and other parts of the system. It is going to be good completion to Apple Back to the Toshiba, I love the way it slides back and forth where you can use it as regular laptop or tablet. The battery life is good and 5 to 6 hours life is good enough for me. It is solid and has a great feel to it where you can take it with you with no worries of dropping it. The 128 GB SS drive plus the Sky drive will hold all my work files and more. Also with Sky drive, you keep all those offline where they are safe in case something happens. If you are in to music it will work for you also. I am not in to gaming that much but it does most of my games good like words with friends and angry birds. The keyboard is great and lights up only when you using it to conserve battery power. One negative I can find is that the battery is internal and just can’t be replaced unless you take apart the computer Once you start learning Windows 8 you will get the hang of it quickly because I am learning different things every day. One thing I just recently learned was in the apps you can find all those other items programs that are offered in Windows 7 like word pad and media player and maintenance functions. The screen size works for me because I watch movies on it when I am on the road from HBO, Netflix and Hulu and definitely like to see it on a bigger screen than say a 7 inch. The Toshiba is a great buy and sure you won’t be disappointed."

Leads the pack with features

POSTED BY: , Baltimore MD
Overall rating: 4.0 out of 5

"What stands out with the U925T is the great feature set. NFC, WiDi, SSD, backlit Keyboard. I've been able to use all these features and it truly makes this device shine What's needed, they MUST ship with Win 8 Pro and not just standard! Need to include a sleeve since you carry it around with the screen exposed all the time."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Satellite Laptops
  • U920t
    Satellite® U920t
    Two devices in one
    Touch screen display
    Pre-loaded with Windows 8
    Ultra light and slim profile
    Built-in entertainment features
    Starts at: $870.99
  • L840L840
    Satellite® L840
    Great for everyday computing
    Easy to carry design
    Fashionable and affordable
    Great for enjoying multimedia
    Preloaded with Windows8
    Starts at: $449.99
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
    Starts at: $779.99
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
    Starts at: $524.99
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
    Starts at: $486.99
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
    Starts at: $679.99
  • S870S870
    Satellite® S870
    Great desktop replacement
    Big screen viewing
    Premium speakers
    Entertainment-focused features
    Preloaded with Windows 8
    Starts at: $524.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.