5 models available
Starting at $849.99
$849.99
POSTED BY:
Kitty
For Model: Satellite U925T-S2130
Overall rating:
4.0 out of 5
"Within the past two months is when I got my new Toshiba laptop and I love it. At first it had some difficulties with Skype but with some online help it was solved. I love how small and thin it is but not overly so. Pretty light and my keys are backlit - cool! =]"
POSTED BY:
The king
For Model: Satellite U925T-S2120
Overall rating:
5.0 out of 5
"Very good machine, 120 GB is not too much but is OK"
POSTED BY:
Andres
,
Texas
For Model: Satellite U925T-S2120
Overall rating:
4.0 out of 5
"Keyboard has a mind of its own. Attempt to Register with Toshiba have fruitless, even after more than half of dozen tries. Camera is so poor, it should not have been included on unit. On a positive side, impressed with speed, colors and general response of unit."
POSTED BY:
MarinePapa
,
Charleston, WV
For Model: Satellite U925T-S2120
Overall rating:
5.0 out of 5
"I got this in about a week ago. I upgraded to Windows 8 Pro and I use a 128 Gig SDXC card for extra storage. I know that some reviews say that Ultrabook Convertibles will not replace a traditional computer, but after setting mine up, I haven't used my old laptop in days. I find it a little more difficult to type, but I easily got used to it. I don't use the mouse very much with Windows 8, but the track pad does come in handy sometimes. I am extremely pleased."
POSTED BY:
Texas Senior
,
Fort Worth TX
For Model: Satellite U925T-S2300
Overall rating:
4.0 out of 5
"The idea of multile positions is good, but is worrisome. The screen is sometimes difficult to handle. I am concerened about the life of the tracks and the hindges."
POSTED BY:
Btween2Evils
,
Alexandria, VA
For Model: Satellite U925T-S2300
Overall rating:
4.0 out of 5
"I love the fact that this product converts from a laptop to a tablet. It's lightweight, easy to use, and the light-up keyboard feature is nice to have. One thing that I would have liked to see is the availability to use the rear-facing camera when the device is collapsed as a tablet. The rear camera is only exposed in laptop mode, making it difficult to snap pictures and hold the device at the same time."
POSTED BY:
alev1275
,
New York, NY
For Model: Satellite U925T-S2300
Overall rating:
3.0 out of 5
"As a longtime slider phone user (need that qwerty keybard!) thought I'd try the U925t as my first Win 8 experience. Feelings mixed so far. As a laptop it's fine, but dark screen & low def make it not great for media. Price also too high for what it is."
POSTED BY:
PattyP
,
Haines, AK
For Model: Satellite U925T-S2300
Overall rating:
5.0 out of 5
"This laptop is so easy to use. I am not very computer tech but have no problems getting where I wish to go. Love the touch screen! And being able to fold it up into a tablet is awesome!"
POSTED BY:
MEKLBD
,
Rome
For Model: Satellite U925T-S2301
Overall rating:
4.0 out of 5
"Toshiba U925T is a very high performing laptop ever I seen. So people can buy it easily."
POSTED BY:
Greg
,
Marion, IL
For Model: Satellite U925T-S2300
Overall rating:
5.0 out of 5
"This has got to be one of the best purchases I ever made! The computer is very light and the new Windows 8 operating system runs fast compared to older versions. Well, I have to admit Windows 7 is great also but this offers much more with the tiles. You have to get this touch screen because trust me, I loaded the trial version of 8 on my other laptop and it’s just not the same using a keyboard and mouse. Granted, it is lacking some apps but more and more are getting added daily. I have tried iPad and this is operating system is going to create havoc for the Apples system. They made many improvements with security with Defender and other parts of the system. I love the way it slides back and forth where you can use it as regular laptop or tablet. The battery life is good and 5 to 6 hours life is good enough for me. It is solid and has a great feel to it where you can take it with you with no worries of dropping it. The 128 GB SS drive plus the Sky drive will hold all my work files and more. Also with Sky drive, you keep all those offline where they are safe in case something happens. If you are in to music it will work for you also. I am not in to gaming that much but it does most of my games good like words with friends and angry birds. The keyboard is great and lights up only when you using it to conserve battery power. One negative I can find is that the battery is internal and just can’t be replaced unless you take apart the computer. Once you start learning Windows 8 you will get the hang of it quickly because I am learning different things every day. One thing I just recently learned was in the apps you can find all those other items programs that are offered in Windows 7 like word pad and media player and maintenance functions. The screen size works for me because I watch movies on it when I am on the road from HBO, Netflix and Hulu and definitely like to see it on a bigger screen than say a 7 inch. The Toshiba is a great buy and sure you won’t be disappointed."