Toshiba Satellite U945-S4380 Laptop

Satellite U945-S4380

MSRP: $699.99
Satellite U945-S4380 4.67 out of 5.0 based on 3 user reviews. Average Customer Rating: 4.67 out of 5.0
Read Reviews (3)  | Write Reviews
Intel® Core™ i3 Processor
Accessories for the Satellite U945-S4380

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

More Satellite U940 Series Laptops
U940
Model: MSRP:
U945-S4110 $499.99
U945-S4130 $511.49
U945-S4140 $612.99
U945-S4380 $699.99
U945-ST4N01 $679.99*
U945-S4390 $799.99
U945-ST4N02 $799.99*

*ToshibaDirect Exclusive. Price includes applicable discounts.

Satellite U945-S4380 Laptop Customer Reviews

I finnd it a perfect companion

POSTED BY: , San Francisco, CA
Overall rating: 5.0 out of 5

"This is my second Toshiba laptop computer. The previous one, a netbook, was excellent too but it had drawbacks that have been improved in the Satellite. Windows 8 is also very nice but Windows 7 is more to my liking. However, there are features in Windows 8 that make it a very nice modern OS and so I highly recommend both. I recommend you upgrade today!"

laptop

POSTED BY: , Michigan
Overall rating: 4.0 out of 5

"I am not excited about windows 8 I guess I should have just went with somethng I already knew windows 7"

Love the laptop

POSTED BY: , York, PA
Overall rating: 5.0 out of 5

"Hate Windows 8, Not the right system for a laptop! The machine is great, light., long battery life."
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
  • U940
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
Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.