Toshiba Tecra M11-S3450 Laptop

Tecra M11-S3450

MSRP: $1,429.00
Tecra M11-S3450 3.50 out of 5.0 based on 4 user reviews. Average Customer Rating: 3.50 out of 5.0
Read Reviews (4) 
This laptop is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
Tecra R940 Series »
Laptop Accessories
Shop for Tecra M11-S3450 accessories at ToshibaDirect.com.
Technical Support
Get support for your Tecra M11-S3450 or try our Laptop Forums for additional help.
Intel® Core™ i7 Processor
This product may be available at a local business reseller.

Find a Reseller

Accessories for the Tecra M11-S3450

Accessories
Carrying Cases
Batteries
AC Adapters
Docking & Expansion

Tecra M11-S3450 Laptop Customer Reviews

Tecra M11 experience

POSTED BY: , Westfield, Indiana
Overall rating: 1.0 out of 5

"Initially, my experience was without problems. However, in the last week to ten days, my problems have consisted of long boot up times, inability access AOL w/o having to reboot several times, inability to open word, and inability to properly load Word 2010. I am unable to access add/remove programs to determine if there are conflicts preventing me from accessing different programs."

Solid Overall Performance

POSTED BY: , los angeles, CA
Overall rating: 4.0 out of 5

"I'm an IT guy for a company in Los Angeles. We recently purchased 2 - M11 models. Our company purchases many Toshiba Laptops each year, and we recently purchased 2 - M11 models. Overall they are one of the best when it comes to business use! Most employees don't take the time to care for their laptop, so it gets kicked around if you know what I mean. But, Toshiba keeps on working even with the abuse! So, they're very solid PCs. The downside lately I find comes down to 2 issues: 1) Battery life: Toshiba batteries don't seem to last very long? You have to replace them anywhere between 18 - 24 months. Toshiba needs to focus on upgrading their battery life. 2) On some of their models, usually their A Series, and sometimes their M Series, there is an issue with the curser moving by itself? This is generaly caused by resting the palms of your hands on the laptop as you type. Toshiba needs to prevent this issue, because many use these laptops when traveling, and especially while on a plane. The reason I gave it 4 Star Overall rating, is because of the poor battery life. But I must say, overall it really is a great laptop!"

Fast, excellent build quality

POSTED BY: , Seattle, WA
Overall rating: 5.0 out of 5

"This is a solidly built laptop with a lovely screen, fast performance, and good ergonomics. The version I'm using has been upgraded to 8 gigabytes of RAM and has an SSD. Boot times are under 30 seconds (including POST). While the i7-620M is a dual core (with hyperthreading), virtual machines are fast and responsive, and allocating two cores to a VM works well. The machine feels like it will actually last the three years on the warranty. At normal font size resolution, the 1600x900 allows for plenty of screen real estate for programming or writing, but remains readable (mileage of course will vary by user). The laptop itself is small and light enough to carry."

Fast but sturdy little beast

POSTED BY: , Portland, OR
Overall rating: 4.0 out of 5

"I am a hardware design engineer and I am always pleased by my Toshibas from a design aspect. I have purchased four of them now and don't plan to change. The M11 is very fast. I initially wanted to get a Portege because they are so very light and visually appealling but the reviews suggested that the fans had to really work overtime (ie very noisy) to handle the faster processors. I didn't think I could deal with noisy so I went with the larger format of the M11 and the noise issue is negliable.....a little louder than my Satellite but not much. I have generally gone with Toshiba's because they are very durable and I am hard on them. I have dropped them, banged them and generally not been very careful. In addition, my puppies have pulled them off desks, chewed their cords....well, let us say we are not a good environment for hardware. Nevertheless, our Toshibas have taken a lickin' and come back fine. Once I spilled a beer on my Toshiba. I dried it out with a hairdryer on low and it was back in a day or so and ran for years. My biggest complaint about the M!! is that I really do not like the speakers. I like to listen to classical music while I work at home and it doesn't sound nearly as good on the M11 speakers as it did on my old Toshiba Satellite. However, a minor thing. The fingerprint scanning is sort of fun but clearly not essential. The standard configuration for the i7 seems to perform very well. No complaints there. Monitor fine, keypad and other entry fine. Format perfect for me, not too big, not too small. Weight acceptable for a 15 inch screen with disk drive on-board. Have to say, I'm happy. The price/performance trade off was reasonable, with a ton of durability thrown in for good measure.""

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Tecra Laptops
  • R940R940
    Tecra® R940
    Highly durable and reliable
    Stylish, easy-to-carry design
    Perfect for mobile professionals
    Full performance laptop
    Extended battery life rating
    Starts at: $599.99
  • R950R950
    Tecra® R950
    Perfect desktop replacement
    Highly durable and reliable
    Ideal productivity laptop
    Extended battery life rating
    A showcase of features
    Starts at: $599.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.