x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Toshiba TransMemory®
USB Flash Drives

starting at: $ Shop USB-FLASH-DRIVES Series

USB Flash Drives

USB Flash Drives

7 models available Starting at $7.79 $7.79
$36.99
USB Flash Drives 3.4 out of 5.0 based on 5 user reviews.

Customer Reviews for USB Flash Drives

Best I've ever owned

POSTED BY: , MO
For Model: Flash THNU58N32GTRT
Overall rating: 5.0 out of 5

"As a student I use flash drives all the time, even when I'm not in school. This is by far the best I've ever used, it's durable, it's fast, and it's got a large capacity. It amuses me when people say it's slow, when it's really their computers that are slow. this is the best flash drive I've ever used, and it probably always will. If I were to somehow destroy this item, I'd buy it again."

bad product

POSTED BY:
For Model: Flash THNU48N16GTRT
Overall rating: 2.0 out of 5

"My Toshiba Flash drive worked for about one year then it just stoped working. I cant format or anything it doesnt show me the flash drive just says put something in G."

Best for the price

POSTED BY: , New Britain, Ct
For Model: Flash THNU48N16GTRT
Overall rating: 5.0 out of 5

"Ease of use -fast and quick Had no problems getting to use it Works fine on all my computers"

Too slow for me!

POSTED BY: , Amsterdam, Netherlands
For Model: Flash THNU48N16GTRT
Overall rating: 2.0 out of 5

"I can copy files to it with a speed of 6.25 MB/Sec. Sometimes a shooter of 7 or 8 MB per sec... It's good for backups, etc. but if you're in a rush and need to copy large files, you're doomed... I can't complain about the reading speed though, that's alright :) It would've been nice if these usb sticks had a minimum of 10 MB/S write speed, then it would've completely been worth it's money."

excellent

POSTED BY: , Indonesia
For Model: Flash THNU58N32GTRT
Overall rating: 3.0 out of 5

"very nice, it's just less speed so fast, it was evident when I tried to move applications from a laptop to a USB drive."

Choose a model to see detailed specs »

starting at:
$
Shop USB-FLASH-DRIVES Series

More Flash
  • Memory CardsMemory Cards
    Memory Cards
    Great for adding storage to portable devices
    Ideal for transferring files
    Available in various capacities
    Very reliable and convenient
    SD & Micro SD cards available
    Starts at: $4.99
  • USB Flash Drives
    USB Flash Drives
    Ideal for transferring files
    Available in various sizes
    Very convenient and reliable
    Downloadable security software
    Starts at: $7.79
  • FlashAir™ WiFi SD CardsFlashAir™ WiFi SD Cards
    FlashAir™ WiFi SD Cards
    Built-in Wi-Fi
    Share memories instantly with multiple devices
    Store photos, videos and files
    8GB of storage
    No software installation needed
    Starts at: $54.99