1TB Canvio® 3.0 Portable Hard Drive (Black)

1TB Canvio® 3.0 Portable Hard Drive (Black)

  • List Price:
  • $129.99

Total Price:

$129.99

Buy Now
Portable HDTC610XK3B1 1.92 out of 5.0 based on 24 user reviews. Average Customer Rating: 1.92 out of 5.0
Read Reviews (24)  | Write Reviews

Storage - HDTC610XK3B1 Product Customer Reviews

Unreliable

POSTED BY: , BVTN, OR
Overall rating: 1.0 out of 5

"Had this bad boy for a little over year. It was used very sparingly as its primary purposed was for occasional data storage. Clicking death, and with it all my data, even though I was very careful while handling it."

ok

POSTED BY: , Santa Barbara
Overall rating: 1.0 out of 5

"I liked Toshiba, until my experiences with the Passport external HD, and various 'facets' of customer 'support' that may, or may not be available. They need to remember that thousands of people bought models previous to canvio, and win 8 in the last six, to eighteen months."

It's perfect until it brakes

POSTED BY: , Ms
Overall rating: 3.0 out of 5

"I had already 2 different Canvio models. They are perfect until they brake. None of them lasted even a year. I hope Toshiba will improve them because they are VERY HANDY."

Worst external HD Ever

POSTED BY: , Ladson, SC
Overall rating: 1.0 out of 5

"got the 1TB because of the price. Don't. Had it less than 3 weeks and filled it halfway up with my Wii, and all the sudden it froze up and died. I tried removing the HD from he enclosure, but f'n Toshiba WELDED the enclosure closed, so I can not even get my data off before returning/trashing. Normally I like Toshiba, but after reading other reviews on the DWC110, DO NOT BUY THIS PRODUCT! ps-another person posted you need USB 3.0. Not true; worked perfect for a while in 2.0, not will not work at all, even in 3.0."

If you do not have 3.0, do not waste your money.

POSTED BY: , NJ
Overall rating: 1.0 out of 5

"This drive does not stay connected unless you have a 3.0 USB connection. The device packaging claims it is capable of USB 2.0 use but it is not. It disconnects at random moments ranging from 10 seconds to 20 minutes."

Junk—Lost Data, Dead Drive

POSTED BY: , Kilgore, TX
Overall rating: 1.0 out of 5

"I placed a fair number of files on this drive from a desktop PC running Win XP SP3. Moved them to a new (Sept 2012) Macbook Pro. Installed the provided software to make the disk R/W from the Mac. Tried writing to the drive and it failed. Now the drive isn't even recognized by ANY Windows or Mac machine. And yes—it's *supposed* to work with a Mac. Thank heavens I back up my work using other hardware, too—but this has trashed the files and lost a bit of work on a legal case. Very expensive."

not a good buy

POSTED BY: , las vegas
Overall rating: 1.0 out of 5

"worked for 3 weeks then died .. computer will not reconize it and i have all my data on it.. any suggestion on how to get my data off?"

Excellent Drive

POSTED BY: , Terre Haute, IN
Overall rating: 5.0 out of 5

"I have used many other Toshiba external drives but read the reviews before I purchased this one. I could disregard all the one star reviews as the problems the users were describing were typical computer software and driver problems, not problems caused by this drive. I have tested this drive on five desktops and four laptops and it works flawlessly."

Just to reiterate

POSTED BY: , Rome Italy
Overall rating: 1.0 out of 5

"Do not purchase,read all the above poor ratings and take your pick!!!Although the drive letter is visable on all 7 of various devices, Mac & PC the archived information is only accessable on ONE of them and then only using USB 2. I'll just repeat ....do not purchase. Ps three of the 7 devices mentioned above are.......Toshiba...go figure!!!"

Awful!!!!

POSTED BY: , Florida
Overall rating: 1.0 out of 5

"Plugged the product in, it said the software was installed but then I wasn't able to access the drive. Tried to uninstall and reinstall with no luck. There is absolutely no support available for this product online and the manual is completely useless. Oh, the manual does tell you if you have problems after installation to just hit the "help" button on the device...too bad I can't even get to that point because the device DOESN'T WORK! I don't have the time to waste on trying to troubleshoot this product and now I have to waste more time returning it and purchasing a new drive. It won't be a Toshiba product. Very unhappy."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portable
  • Canvio® Basics 3.0Canvio® Basics 3.0
    Canvio® Basics 3.0
    Blazing-fast transfer speeds
    Simple add-on storage
    Drag-and-drop convenience
    Various capacities
    Three-year limited warranty
    Starts at: $89.99
  • Canvio® 3.0
    Canvio® 3.0
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Choice of cool colors
    Three-year limited warranty
    Starts at: $99.99
  • Auto Backup HDDAuto Backup HDD
    Auto Backup HDD
    Very easy to use
    Automatically backs-up files
    No software to install
    Fast transfer speed
    Choice of colors & capacities
    Starts at: $109.99
  • Canvio® SlimCanvio® Slim
    Canvio® Slim
    Slim design, perfect for Ultrabook PCs
    Pre-loaded backup software
    Customizable backup routine
    Built-in USB 3.0 Interface
    PC and Mac compatible
    Starts at: $114.99
  • Canvio<sup>®</sup> ConnectCanvio<sup>®</sup> Connect
    Canvio® Connect
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Easy set-up
    Various colors available
    Starts at: $99.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.