1TB Canvio® 3.0 Portable Hard Drive (Silver)

1TB Canvio® 3.0 Portable Hard Drive (Silver)

  • List Price:
  • $129.99

Total Price:

$129.99

Buy Now
Portable HDTC610XS3B1 2.08 out of 5.0 based on 13 user reviews. Average Customer Rating: 2.08 out of 5.0
Read Reviews (13)  | Write Reviews

Storage - HDTC610XS3B1 Product Customer Reviews

Good little HDD

POSTED BY: , Henderson, KY
Overall rating: 4.0 out of 5

"I purchased this 1TB portable disk drive to back up my laptop after learning the hard way the dangers of not backing up my files. It worked right from the start, not exactly the fastest backup, but hardly slow either, backed up faster than my friend's computer running same OS (Windows 7 64-bit) and I have USB 2.0 on my laptop. Our computer hard drives are both 250GB as well. I went for a bit of overkill on my portable drive in case I every replace my computer and that has a larger hard drive."

Does not work on all LTs

POSTED BY: , Bath, PA.
Overall rating: 1.0 out of 5

"I bought this because the Name and Price and warranty. I am contacting Toshiba to let them know my dissatisfaction. Works on my HP 3.0 USB LT Wont work on my HP 2.0 USB LT. I cannot confirm on other USB 2.0 but it seems I need a special cable to use it.ETITHER PUT IT IN THE BOX OR LABLE IT AS SUCH If all you are gonna use it for is USB 3 you will love this unit. Priced right with 3 yr warranty beats the compitition hands down. If you ever think you may take it to a friend be warned. IF he has an old pc/lt you may not be able to share data."

Worked like a charm

POSTED BY: , Texas
Overall rating: 4.0 out of 5

"I bought it to back up my imac. My mac knew the drive had to be reformatted, then asked if I wanted to use it as a time machine and presto! I was done with TB of back up. Also, there is no need to plug it in for electricity, it runs off your USB."

Doesn't even start

POSTED BY:
Overall rating: 1.0 out of 5

"Driver wouldn't install after plugging into the third computer, it installed then it shut itself off. Doesn't show up as a drive. I have to return to the store since it never even manifested itself."

Great Experience! So far so good.

POSTED BY: , Hartford, CT
Overall rating: 4.0 out of 5

"Just bought it for my iMac and did the first backup using Time Machine (TM)... It was so easy. TM identified it and asked if I wanted to use it as a backup device, I said yes. It asked if I really wanted to erase and reformat the disk. This is the only reason I don,t give it 5 stars, it erased all the software that came with the HD. However, if using TM, you don,t need the preinstalled software. I then scheduled my backup, and presto, within less than an hour it was done. Easy to use and great value."

DONT BUY!

POSTED BY: , McAllen, TX
Overall rating: 1.0 out of 5

"What a piece of junk! Plugged it into a TOSHIBA laptop and created a couple of backup directories. Second file transferred caused an over-current shutdown and now the drive cannot be copied to. Run, as if your life depended on it, away from this piece of junk. I read the "junky cable" reviews and plugged it into a seldom used USB port, so I KNOW the port connector is good. I don't think that that is the problem. I don't think I'll ever buy another Toshiba product after they released this piece of junk!"

Doesn't work wwith my I Mac

POSTED BY: , Bremerton Wa
Overall rating: 1.0 out of 5

"Bought this to back up my I Mac before upgrading my system, Plug it in couldn't get it do anything, has no instructions on how to back up, so if your no computer savy your screwed, will be brining this back . Don't waste your money if you have a Mac."

Returning to store

POSTED BY: , Newport News, VA
Overall rating: 1.0 out of 5

"This drive was bought to backup my MacBook Pro. It worked with an earlier version of the pro but the newer versions will hang for a few seconds and the drive never shows up. I tried different variations on getting it to be properly seen by the laptop but had no luck. I will be returning this drive to the store today. Just be careful and read reviews before purchasing."

Connector not working properly

POSTED BY: , ny
Overall rating: 1.0 out of 5

"Returning to store. Connector needs to be held in place to work properly. Wish I had read other reviews before buying this."

Doesn't work with my new MacBook Pro

POSTED BY:
Overall rating: 2.0 out of 5

"I understand that this disk needs to be reformatted in order to work with a Mac. However the Disk Utility on my new 15" MacBook Pro doesn't even see this disk. The computer hangs for many seconds when I connect the disk. There seems to be some fundamental incompatibility. The disk works just find on my Lenovo laptop running Windows XP. I wish I knew what the problem was with my Mac."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portable
  • Canvio® Basics 3.0Canvio® Basics 3.0
    Canvio® Basics 3.0
    Blazing-fast transfer speeds
    Simple add-on storage
    Drag-and-drop convenience
    Various capacities
    Three-year limited warranty
    Starts at: $89.99
  • Canvio® 3.0
    Canvio® 3.0
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Choice of cool colors
    Three-year limited warranty
    Starts at: $99.99
  • Auto Backup HDDAuto Backup HDD
    Auto Backup HDD
    Very easy to use
    Automatically backs-up files
    No software to install
    Fast transfer speed
    Choice of colors & capacities
    Starts at: $109.99
  • Canvio® SlimCanvio® Slim
    Canvio® Slim
    Slim design, perfect for Ultrabook PCs
    Pre-loaded backup software
    Customizable backup routine
    Built-in USB 3.0 Interface
    PC and Mac compatible
    Starts at: $114.99
  • Canvio<sup>®</sup> ConnectCanvio<sup>®</sup> Connect
    Canvio® Connect
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Easy set-up
    Various colors available
    Starts at: $99.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.