1.5TB Canvio® 3.0 Portable Hard Drive (Black)

1.5TB Canvio® 3.0 Portable Hard Drive (Black)

  • List Price:
  • $169.99

Total Price:

$169.99

Buy Now
Portable HDTC615XK3B1 2.60 out of 5.0 based on 5 user reviews. Average Customer Rating: 2.60 out of 5.0
Read Reviews (5)  | Write Reviews

Storage - HDTC615XK3B1 Product Customer Reviews

ZERO Documentation!

POSTED BY: , Sacramento CA
Overall rating: 1.0 out of 5

"It's hard to rate using the star system above, since there's absolutely NOTHING included with this drive that tells me ANYTHING, other than one page in the user guide (out of 34, the rest are for different languages) that basically just spells out what's included and the warranty. Give us some insight - this is ridiculous."

Connection

POSTED BY: , TX
Overall rating: 2.0 out of 5

"using windows 8 I connected to the usb and nothing happens, I tried a lot of times and finally... something needs to be fixed.. :-S"

Ok Back Up Drive

POSTED BY: , Missouri
Overall rating: 3.0 out of 5

"If you use the pass code feature - you can not unlock the drive and just see what files are on the drive - it only gives you the option to back up you files or restore your files - this drive does not allow you just to look at whats on the drive if you use a pass code feature - other then that it does what it is made to do and that is back up your files or restore your files - it does not come with a users guide that tells you how to use the drive - and if you want to back up your files and see whats on the drive you have to do it without using a pass code feature and that is not secure - this device needs a little more thinking put into the design coming from a company that has leading innovation in its company name - bought this back up drive on 02162013"

Just what you need

POSTED BY: , Porto Alegre
Overall rating: 5.0 out of 5

"I really enjoy my Canvio hard drive. It fits in my pocket and I still haven't found a computer or device that doesn't recognize it immediately. Moving media between my notebook and my PS3 was never easier. Be careful with one thing: they are so small and light I usually forget they are attached to my notebook. Well, luckily they are so light the USB cable holdes them and they don't fall off."

Really?

POSTED BY: , Military, Italy
Overall rating: 2.0 out of 5

"Not able to link up to my PC. Have to try, try and try again, restarting, shutting down, etc to get it to catch. Not sure what the problem is. Once it links up to my computer, it's solid, but the time it takes to get there is not so impressive."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portable
  • Canvio® Basics 3.0Canvio® Basics 3.0
    Canvio® Basics 3.0
    Blazing-fast transfer speeds
    Simple add-on storage
    Drag-and-drop convenience
    Various capacities
    Three-year limited warranty
    Starts at: $89.99
  • Canvio® 3.0
    Canvio® 3.0
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Choice of cool colors
    Three-year limited warranty
    Starts at: $99.99
  • Auto Backup HDDAuto Backup HDD
    Auto Backup HDD
    Very easy to use
    Automatically backs-up files
    No software to install
    Fast transfer speed
    Choice of colors & capacities
    Starts at: $109.99
  • Canvio® SlimCanvio® Slim
    Canvio® Slim
    Slim design, perfect for Ultrabook PCs
    Pre-loaded backup software
    Customizable backup routine
    Built-in USB 3.0 Interface
    PC and Mac compatible
    Starts at: $114.99
  • Canvio<sup>®</sup> ConnectCanvio<sup>®</sup> Connect
    Canvio® Connect
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Easy set-up
    Various colors available
    Starts at: $99.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.