500GB Canvio® Basics 3.0 Portable Hard Drive (Black)

500GB Canvio® Basics 3.0 Portable Hard Drive (Black)

  • List Price:
  • $89.99

Total Price:

$89.99

Buy Now
Portable HDTB105XK3AA 2.35 out of 5.0 based on 20 user reviews. Average Customer Rating: 2.35 out of 5.0
Read Reviews (20)  | Write Reviews

Storage - HDTB105XK3AA Product Customer Reviews

Intermitent Cable

POSTED BY: , Michigan
Overall rating: 1.0 out of 5

"The main issue I have withthe product is the connector on the HD is intermitent. I would like to see Toshiba send out a replacement cable to their customers that fixes the problem."

Not bad

POSTED BY: , Toronto
Overall rating: 5.0 out of 5

"I have 2 of those. No problem after using for 2 or 3 years."

Excellent Portable Drive!

POSTED BY: , Dayton, OH
Overall rating: 5.0 out of 5

"Worked perfect straight out of the box! No software pre-installed to hog up space - very nice!!"

Great little drive

POSTED BY: , Iowa
Overall rating: 5.0 out of 5

"Read reviews, do not understand the poor reviews.I own 2 of these. One for system backup on win 7, the other for files on both 2.0 and 3.0 systems. I have win7 pro 64, Quad Xeon system and XP system. Plugged it in, works. I do not install the software on the drive. See no need for it."

Toshiba Canvio 3.0

POSTED BY: , San Jose Ca
Overall rating: 1.0 out of 5

"Bought it, plugged it in. Nothing. No directions. Looked at the web site. Horrible reviews and same complaint. Put it back in the box and will return. Waste of time and gas. Who ever heard of a product with no information on it in the package? Strange..."

Hate it

POSTED BY: , Bradenton, FL
Overall rating: 1.0 out of 5

"Just bought it 2 hours ago and already hate it. others i have purchased were easy as one two three, plug and play and all i wanted was to use as storage."

Stopped working

POSTED BY: , Mill Valley,ca
Overall rating: 1.0 out of 5

"Stopped workin after a couple months, plug it in it spins then turns itself off. Not recognized, Put less than 100g on it and won't work. Very dissapointed in Toshiba."

Failed - same as others have

POSTED BY: , Okalhoma
Overall rating: 1.0 out of 5

"after using to backup a large quantity of data, it was not recognized by any operating systems that I tried, and would not recover. Lasted three months, just long enough to cause me serious problems...."

Toshiba Is The Best

POSTED BY: , New Jersey
Overall rating: 4.0 out of 5

"Very Nice External HD & I Love it."

Great little drive, seamless with OSX

POSTED BY: , Wellington, New Zealand
Overall rating: 5.0 out of 5

"Great drive, I love the fact it's got a shock sensor and ramp loading technology. Many other big players such as WD and Seagate don't offer this on their budget drives. I love the simplicity and small size of the Canvio. It works seamlessly with OSX Snow Leopard formatted for HFS+. Many people are blaming Windows for not detecting it, I say if you buy a cheap computer with a rubbish OS don't blame the HDD, blame the operating system for not including drivers and support for a basic HDD. With the shock sensor, ramp loading system and 3 year warranty I think it's a pretty safe buy if you're concerned about reliability. As with any hard disk drive you've gotta be careful and not move it while in use otherwise it'll be toast! But so far so good."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portable
  • Canvio® Basics 3.0
    Canvio® Basics 3.0
    Blazing-fast transfer speeds
    Simple add-on storage
    Drag-and-drop convenience
    Various capacities
    Three-year limited warranty
    Starts at: $89.99
  • Canvio® 3.0Canvio® 3.0
    Canvio® 3.0
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Choice of cool colors
    Three-year limited warranty
    Starts at: $99.99
  • Auto Backup HDDAuto Backup HDD
    Auto Backup HDD
    Very easy to use
    Automatically backs-up files
    No software to install
    Fast transfer speed
    Choice of colors & capacities
    Starts at: $109.99
  • Canvio® SlimCanvio® Slim
    Canvio® Slim
    Slim design, perfect for Ultrabook PCs
    Pre-loaded backup software
    Customizable backup routine
    Built-in USB 3.0 Interface
    PC and Mac compatible
    Starts at: $114.99
  • Canvio<sup>®</sup> ConnectCanvio<sup>®</sup> Connect
    Canvio® Connect
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Easy set-up
    Various colors available
    Starts at: $99.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.