750 GB Canvio® Basics 3.0 Portable Hard Drive (Black)

750 GB Canvio® Basics 3.0 Portable Hard Drive (Black)

  • List Price:
  • $99.99

Total Price:

$99.99

Buy Now
Portable HDTB107XK3AA 2.83 out of 5.0 based on 5 user reviews. Average Customer Rating: 2.83 out of 5.0
Read Reviews (5)  | Write Reviews

Storage - HDTB107XK3AA Product Customer Reviews

USB External hard drive / back up

POSTED BY: , Topeka Kansas
Overall rating: 5.0 out of 5

"Been using my external hard drive and back up for the last four years now. I use it as a separate drive so store family photos and other items that I just don't want to loose due to computer failure. I manually control back ups so not using the back up software other than on my command but the device itself has worked flawlessly since installed. Running with Windows Vista 64 bit OS. Wanting to purchaser a second one because the original is about 90% full."

Decent Backup HD for the $$

POSTED BY: , Minneapolis, MN
Overall rating: 4.0 out of 5

"After reading through several less than favorable reviews, I decided to read the online user guide and Q&A's. Many of the bad reviews appear to be "user error." A good example is the review that says it doesn't work on Windows 7 64 bit. The Q&A and user guide answered this question as listed below, and was exactly how it operated on my Windows 7 64 bit machine. Q: How do I begin the installation of the NTI software? A: When you connect the Toshiba USB hard drive the AutoPlay function of Windows XP & Vista will prompt you to install backup software. Note: Windows 7 and Windows 8 do not allow USB hard drives to AutoPlay. You will only be prompted to open the drive to view files or use this drive for backup. In this case, select Use this drive for backup. Unless you are at least a proficient user of computer hardware, I highly encourage reading materials before trying to operate."

Worst money waster ever

POSTED BY: , Canada
Overall rating: 1.0 out of 5

"Not compatible with Windows 7 64 bit. DO NOT BUY THIS HARDDRIVE"

great

POSTED BY:
Overall rating: 5.0 out of 5

"perfect for me to store all my movies on it and keep a backup of my computer"

Don't buy

POSTED BY: , Coral Springs FL
Overall rating: 1.0 out of 5

"2 words NO GOOD"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Portable
  • Canvio® Basics 3.0
    Canvio® Basics 3.0
    Blazing-fast transfer speeds
    Simple add-on storage
    Drag-and-drop convenience
    Various capacities
    Three-year limited warranty
    Starts at: $89.99
  • Canvio® 3.0Canvio® 3.0
    Canvio® 3.0
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Choice of cool colors
    Three-year limited warranty
    Starts at: $99.99
  • Auto Backup HDDAuto Backup HDD
    Auto Backup HDD
    Very easy to use
    Automatically backs-up files
    No software to install
    Fast transfer speed
    Choice of colors & capacities
    Starts at: $109.99
  • Canvio® SlimCanvio® Slim
    Canvio® Slim
    Slim design, perfect for Ultrabook PCs
    Pre-loaded backup software
    Customizable backup routine
    Built-in USB 3.0 Interface
    PC and Mac compatible
    Starts at: $114.99
  • Canvio<sup>®</sup> ConnectCanvio<sup>®</sup> Connect
    Canvio® Connect
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Easy set-up
    Various colors available
    Starts at: $99.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.