x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Canvio® Basics 3.0
Portable Hard Drives

starting at: $ Shop CANVIO-BASICS Series

Canvio® Basics 3.0

6 models available Starting at $89.99 $89.99
$189.99
Canvio® Basics 3.0 2.46 out of 5.0 based on 76 user reviews.

Customer Reviews for Canvio® Basics 3.0

Intermitent Cable

POSTED BY: , Michigan
For Model: Portable HDTB105XK3AA
Overall rating: 1.0 out of 5

"The main issue I have withthe product is the connector on the HD is intermitent. I would like to see Toshiba send out a replacement cable to their customers that fixes the problem."

USB External hard drive / back up

POSTED BY: , Topeka Kansas
For Model: Portable HDTB107XK3AA
Overall rating: 5.0 out of 5

"Been using my external hard drive and back up for the last four years now. I use it as a separate drive so store family photos and other items that I just don't want to loose due to computer failure. I manually control back ups so not using the back up software other than on my command but the device itself has worked flawlessly since installed. Running with Windows Vista 64 bit OS. Wanting to purchaser a second one because the original is about 90% full."

Not good

POSTED BY: , ms
For Model: Portable HDTB115XK3BA
Overall rating: 1.0 out of 5

"It worked for 10 months. It is perfect as long as it works but it will brake eventually and sooner then you expect. It was the second failure Canvio model I bought. No more risk."

piece of junk

POSTED BY:
For Model: Portable HDTB110XK3BA
Overall rating: 1.0 out of 5

"won't recognize windows 7. so stupid this hard drive"

Awesome product.

POSTED BY: , Henderson, CO.
For Model: Portable HDTB120XK3CA
Overall rating: 5.0 out of 5

"I bought this for my Wii U to have seemingly endless memory. I recommend using a y-cable for any other device you may use this for, but a y-cable is required for use on Wii U(uses USB 2.0). It reads fast and is very compact. I had the bigger self powered model, and I returned it with the warranty, because it was making clicking noises and reading kinda slow. Get this one if you can, and make sure to get a y-cable if you are using USB 2.0. Also, do more research if you are buying for MAC. Apple makes their own special products usually, and it can be hard to shop PC components most of the time. I'm pretty sure this will work on older MAC computers, but newer ones have more compatibility issues it seems. Overall, I am very satisfied with this product. It has a shock absorber for falls and movements during use, but I am careful with my stuff and will not test it."

Fast but Delicate

POSTED BY: , Nebraska
For Model: Portable HDTB110XK3BA
Overall rating: 2.0 out of 5

"I have now owned two of these and have had to return both within about two to three months of ownership a piece because with out dropping them they have started to make strange noises, have a hard time connecting to my computer, and corrupting data. I cannot recommend this HD when there are better out there"

Not bad

POSTED BY: , Toronto
For Model: Portable HDTB105XK3AA
Overall rating: 5.0 out of 5

"I have 2 of those. No problem after using for 2 or 3 years."

Back up not available suddenly today

POSTED BY: , Sandy, UT
For Model: Portable HDTB110XK3BA
Overall rating: 1.0 out of 5

"Have been using the USB 2.0 function on my Acer laptop to run back on Norton Security Suite up to today and now that drive is not available for backup. What happen. I have done everything I know to get windows 7 64 bit to recognize the drive to no avail. lap doesn't have usb 3.0 port."

worst product

POSTED BY: , india
For Model: Portable HDTB110XK3BA
Overall rating: 1.0 out of 5

"after few months. it gets disconnected automatically. i have to keep it in particular standing position then only it gets detected. if minor shake is the reason for getting away from that particular standing position then drive gets disconnected. I have another external hard drive from Transcend, and it rocks. 5 years no problem to transcend hdd"

Excellent Portable Drive!

POSTED BY: , Dayton, OH
For Model: Portable HDTB105XK3AA
Overall rating: 5.0 out of 5

"Worked perfect straight out of the box! No software pre-installed to hog up space - very nice!!"

Choose a model to see detailed specs »

starting at:
$
Shop CANVIO-BASICS Series

More Portable
  • Canvio® Basics 3.0
    Canvio® Basics 3.0
    Blazing-fast transfer speeds
    Simple add-on storage
    Drag-and-drop convenience
    Various capacities
    Three-year limited warranty
    Starts at: $89.99
  • Canvio® 3.0Canvio® 3.0
    Canvio® 3.0
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Choice of cool colors
    Three-year limited warranty
    Starts at: $99.99
  • Auto Backup HDDAuto Backup HDD
    Auto Backup HDD
    Very easy to use
    Automatically backs-up files
    No software to install
    Fast transfer speed
    Choice of colors & capacities
    Starts at: $109.99
  • Canvio® SlimCanvio® Slim
    Canvio® Slim
    Slim design, perfect for Ultrabook PCs
    Pre-loaded backup software
    Customizable backup routine
    Built-in USB 3.0 Interface
    PC and Mac compatible
    Starts at: $114.99
  • Canvio<sup>®</sup> ConnectCanvio<sup>®</sup> Connect
    Canvio® Connect
    Blazing-fast transfer speeds
    Pre-loaded backup software
    Cloud-capable
    Easy set-up
    Various colors available
    Starts at: $99.99